STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using an STM32F030F4 20-pin for a battery powered application with just a low quiescent touch tensor (active high) for wake-up from low power stand-by on low-to-high and high-to-low sensor edges.

I'm considering an STM32F030F4 20-pin for a battery powered application. Might a low quiescent touch sensor (output high) in conjunction with the timers/functions onboard the chip be used to wake the chip from low power stand-by on the rising and fal...

How to see a graph from an array?

Hi all,I'm taking a lot of readings from the ADC, and store those reads in an array (reads[2000]).Is there a way to sohw a graph from the reads, using STMStudio or another program?

JAlca by Senior
  • 1335 Views
  • 1 replies
  • 0 kudos

Regarding SPI DMA Rx issue when using SPI 8 bit mode

Hello,I have had an issue with SPI Rx DMA. In short, I recieve twice as many bytes as I expect when using SPI 8 bit mode (STM32CubeIDE setting), but not in 16 bit mode.A brief description of the project:Im using an external accelerometer with 220ksps...

AAnn? by Associate
  • 921 Views
  • 1 replies
  • 0 kudos

Is STM32H743ZIT6 multicore or not

When I read the datasheet, the introduction doesn't mention the number number of cores. Digikey says this is a multicore chip. Mouser doesn't either talk about multicore.Several pages down (14) on the datasheet I can read that this is indeed a multic...

LMI2 by Lead
  • 2032 Views
  • 5 replies
  • 0 kudos

STM32F446ZE doesn't enter in Standby mode

Hi,I am using Standby mode on STM32F446ZE, but I faced with a problem. Sometimes MCU doesn't enter in this mode. Exiting Standby mode via RTC wakeup.Below is present steps which I perform for entering StandbySCB->SCR |= 0x00000004;PWR->CR |= 0x000000...

Resolved! PWM capture using Rising, falling EXTI

Hi all,I am capturing 10 pwm pulses from proximity sensors by making the all pwm pins in rising falling interrupt mode.PWM is captured by a timer at every 100us interrupt.some times pulses are missing, I don't know why this is happening.I am sharing ...

gladdy by Associate II
  • 4754 Views
  • 10 replies
  • 0 kudos

How to use Rotary Encoder effectively in external interrupt

Hi there this is Akash, I am doing a project on STM32F100RB Discovery Kit, in this project I am controlling stepper motor with some parameter given by the user using rotary encoder, basically I want to run the motor in the while loop, and through ext...

Akash R by Associate II
  • 2614 Views
  • 4 replies
  • 0 kudos