STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 - start a RAM image

Hi all,I would like to boot a RAM image. A simple bootloader in flash reads in a linear binary from external spi flash. The RAM image works fine if I load it directly to (AXI)RAM (with JTAG).But when loaded by the boot loader, it does not work (loops...

Microman by Associate III
  • 826 Views
  • 1 replies
  • 0 kudos

Init RCC on a STM32F3 (SOLVED)

------------------------------------------------------------------The init of RCC was correct. The SystemCoreClock variable dont reflect the new frecuency changes still "SystemCoreClockUpdate" is called.-----------------------------------------------...

JAlca by Senior
  • 1067 Views
  • 0 replies
  • 0 kudos

Why don't you make a better debugger than STM-STUDIO?

Some time ago I tried your STM-STUDIO: I found it very rough and can only be used for laboratory debugging.Why don't you plan to build a more flexible debugger that can then be used by the end customer to view internal data or change parameters?If yo...

Configuring interrupt pin using CMSIS

Currently I am trying to configure a second interrupt pin using CMSIS.SYSCFG->EXTICR[1] = (SYSCFG->EXTICR[1] & ~SYSCFG_EXTICR2_EXTI6)|(0b0000 << SYSCFG_EXTICR2_EXTI6_Pos); EXTI->FTSR = EXTI_FTSR_TR6; EXTI->RTSR = EXTI_RTSR_TR6; EXTI->IMR = EXTI_IMR_M...

Emper by Associate II
  • 2854 Views
  • 6 replies
  • 0 kudos

Data convert in to zip format

hi i want to compress the text file in to .zip format and save this in to SD card, could you please tell me any one know about any library that available to do compressingi want .zip, i found some library to do gzipplease suggest me, Thanks in advan...

STM32F745 IWDG Refresh Problem when IWDG_RLR is less than 4

Dear All,I am trying to use IWDG for STM32F745 and I did actually. I used CT Cube MX to configure it. Prescaler is 4, Window is 4095 and RLR is 3. I checked clock configuration and IWDG uses 32kHz RC internal oscillator and count down from RLR. I exp...

0690X00000AtPm5QAF.png 0690X00000AtPm0QAF.png
TA1 by Senior
  • 1240 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 use SPI implement SWD?

I want to use SPI implement SWD protocol. Found this one enter link description hereIs there any advice you can provide detail?Have a nice day

YiKai by Associate II
  • 7206 Views
  • 15 replies
  • 0 kudos