STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

f103 LL spi DMA not interrupted

hii use f103 to read ad7606 with spi i see cube example for LL( hal spi has delay)i want read two out of a2d so i config spi1 master receiver and spi2 slave receiver clk of spi1 and spi2 and a2d connect together out A connect to spi 1 and out 2 conn...

MacLaren by Associate III
  • 837 Views
  • 0 replies
  • 0 kudos

STM32F030F4P6 EMI problems?

Hi,I designed a board with a STM32F030F4P6 on it. The board is about 68x48 mm and contains the microcotroller a AC/DC supply and a nRF24L01 RF-Module. supplied directly with about 5V from an external supply the circuit works as it should. But when I ...

Mister232 by Associate II
  • 8075 Views
  • 9 replies
  • 0 kudos

Entering the Stop modes

Hello,I am using STM32L476 and I was just wondering how do I enter in various stop mode (modes 0, 1 and 2) please?Thanks,ALi.

mmsya by Associate II
  • 1236 Views
  • 1 replies
  • 0 kudos

STM32H753

Can anyone share project stm32h753vi with ethernet RMII ? Thanks so much

unknown memory region

I used mac and st-flash v1.5.1 to download .bin file to B-L475E-IOT01A1, but I got "unknown memory region", could anyone help me to solve this? Thanks

wxie by Associate II
  • 3039 Views
  • 4 replies
  • 0 kudos

Which MCUs support 32.768MHz in SAI slave mode?

I have been trying to get the AD7768-4 to work with an L431.I (belately) realized that the maximum SAI slave clock speed in the L4 is 25MHz. It appears that the APB1 clock speed is the limiting factor. I could potentially achieve 192ksps by replacing...

0690X00000BuyMNQAZ.png