STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Integration of real time data.

Hello,I am trying to estimate soc by coulomb counting method.In coulomb counting we required integration of discharge current.I am getting accurate discharge current but unable to add them by using array. I tried using array :float buffer[50]; float ...

Mohan1 by Associate III
  • 1223 Views
  • 2 replies
  • 0 kudos

sprintf causes hard fault.

I use "sprintf (string,"comment"); everywhere now for some reason, I am getting a hardfault. in an innocuous print.length += sprintf(String + length, "Received Packet from ");length is only 15.String is declared as char String[256];I guess it is us...

Where does my const array go? (memory type?)

So, if we have a large amount of hard coded data we want to incorporate into my program, my presumption was that a const array would allow the compiler to treat the data more like code, than data, in terms of cost against your CPU limits.This was alm...

Power pins of STM32F103RDT6

 Hi,I am using STM32F103RDT6. Kindly suggest me LDO for convert 5 to 3.3V and details regarding decaps values for the all supply line of STM32.

Mom.1 by Associate II
  • 1668 Views
  • 3 replies
  • 0 kudos

Sampling rate calculation of STM32F7 ADC with GPIO Toggling

Hi,I use internal ADC of the STM32F767 microprocessor. I set the ADC parameters like this,static void MX_ADC2_Init(void) {   /* USER CODE BEGIN ADC2_Init 0 */   /* USER CODE END ADC2_Init 0 */   ADC_ChannelConfTypeDef sConfig = {0};   /* USER...

AE104 by Senior
  • 887 Views
  • 2 replies
  • 0 kudos