ADC Stops in between without any error code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-07 5:00 AM
Hello,
I'm using STM32f723ZE controller & ADC configured as follow with external trigger(Timer), I verified timers works properly all the times and ADC 1 Stops after few minutes of data capture, but no error code set in Register.
ADC1 & ADC2; (External Trigger is Timer 8)
ADC1, ADC2 Configured as Dual Mode with DMA Enable (12Bit ADC) + TIM8 & ADC 3 As MultiBuffer with DMA + TIM4
ADC1: (500KHz Sampling Frequency )
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T8_TRGO;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
multimode.Mode = ADC_DUALMODE_INTERL;
multimode.DMAAccessMode = ADC_DMAACCESSMODE_2;
multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_7CYCLES;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
ADC2:
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.ScanConvMode = DISABLE;
hadc2.Init.ContinuousConvMode = DISABLE;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DMAContinuousRequests = ENABLE;
hadc2.Init.EOCSelection = ADC_EOC_SEQ_CONV;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
ADC1 DMA:
hdma_adc1.Instance = DMA2_Stream0;
hdma_adc1.Init.Channel = DMA_CHANNEL_0;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_adc1.Init.Mode = DMA_CIRCULAR;
hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;
hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_adc1.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_adc1.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_adc1.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
/* DMA2_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 1, 1);
HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
ADC3: (External Trigger is Timer 4)
hadc3.Instance = ADC3;
hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc3.Init.Resolution = ADC_RESOLUTION_12B;
hadc3.Init.ScanConvMode = ENABLE;
hadc3.Init.ContinuousConvMode = DISABLE; //DISABLE;
hadc3.Init.DiscontinuousConvMode = DISABLE;
hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING; //ADC_EXTERNALTRIGCONVEDGE_RISING; //
hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T4_CC4; // ADC_EXTERNALTRIGCONV_T8_TRGO;
hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc3.Init.NbrOfConversion = 4;
hadc3.Init.DMAContinuousRequests = ENABLE;
hadc3.Init.EOCSelection = ADC_EOC_SEQ_CONV;
if (HAL_ADC_Init(&hadc3) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_REGULAR_RANK_1;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfig.Channel = ADC_CHANNEL_15;
sConfig.Rank = ADC_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
ADC3 DMA:
hdma_adc3.Instance = DMA2_Stream1; //DMA2_Stream2;
hdma_adc3.Init.Channel = DMA_CHANNEL_2;
hdma_adc3.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc3.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc3.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc3.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; //DMA_PDATAALIGN_WORD;
hdma_adc3.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; //DMA_MDATAALIGN_WORD;
hdma_adc3.Init.Mode = DMA_CIRCULAR;
hdma_adc3.Init.Priority = DMA_PRIORITY_LOW;
hdma_adc3.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_adc3.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_adc3.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_adc3.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_adc3) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc3);
/* DMA2_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 2, 1);
HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
START:
ADC1: (500KHz Sampling Frequency )
unsigned short dmaBuffer[512];
if (HAL_ADCEx_MultiModeStart_DMA(&hadc1, (uint32_t *)&dmaBuffer[0], 64) != HAL_OK)
{
/* Start Error */
_Error_Handler(__FILE__, __LINE__);
}
/* Start ADC PWM generation */
if(HAL_TIM_PWM_Start(&htim8, TIM_CHANNEL_4))
{
/* Counter Enable Error */
_Error_Handler(__FILE__, __LINE__);
}
ADC3: (50KHz Sampling Frequency )
unsigned short pdmaBuffer[512];
halErr=HAL_ADC_Start_DMA(&hadc3, (uint16_t*)&pdmaBuffer[0], 256);
if(halErr!= HAL_OK)
{
Error_Handler();
}
halErr=HAL_DMAEx_MultiBufferStart_IT(&hdma_adc3, (uint32_t)&hadc->Instance->DR, (uint32_t)&pdmaBuffer[0],(uint32_t)&pdmaBuffer[256], 256);
if(halErr != HAL_OK)
{
Error_Handler();
}
}
if(HAL_TIM_PWM_Start(&htim4, TIM_CHANNEL_4) != HAL_OK)
{
/* Counter Enable Error */
Error_Handler();
}
Please let me know, if any issue with following configuration and any light on "why ADC 1 stops after few minutes of data capture & ADC 3 runs as expected ?"
Thanks In Advance
- Labels:
-
ADC
-
DMA
-
STM32F7 Series
-
TIM