STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug: RM0383 Reference manual

In RM0383 Reference manual on page 215 - Section: Continuous conversion mode.There is "SWSTRT bit" but shoul be "SWSTART bit".This is very important bit :-).

JSzem.1 by Associate II
  • 1771 Views
  • 3 replies
  • 1 kudos

ST, please unify the family graphics

On the individual families webpages, there's a clickable image-map, as a table of subfamilies together with their most prominent features.Recently, these underwent a facelift. Unfortunately, in some of them, the subfamilies are ordered top-to-bottom ...

0693W000000VZCsQAO.jpg 0693W000000VZEZQA4.jpg

Will my H743 chip handle 2 x 24 MHz, driven by 2 x SDI?

I have a Nucleo H743ZI2. I have been reading "Mastering STM32" by Carmine Noviello, and on page 188 (last paragraph) he says that the maximum IO toggle rate is 10 MHz on the STM32F446. He gives oscilloscope traces, but I can't see the frequency, beca...

MEwen.1 by Associate II
  • 4840 Views
  • 10 replies
  • 0 kudos

STM32F769 Disco DFSDM with DMA Maximum Transfer Length

Hello,Currently I am working on STM32F769 DISCO board with STM32CubeIDE, my aim is to transfer DFSDM conversion results to FMC RAM using DMA. I am able successfully transfer data and verify it. However, when my total conversion length goes above a li...

FP AI Sensing enable UART printf issue - sensortile

Halo,I am using sensortile and currently trying to be familiar with FP AI Sensing. There is an instruction to enable SENSING1_USE_PRINTF in SENSING1_config.h. I did enable it, however there is an error during compilation, and to solve I need to put S...

HKart by Associate II
  • 3610 Views
  • 6 replies
  • 1 kudos

Can I2C be assigned on CM4 and CM7 separately on STM32H747?

Hello, I am new to ST micro controller. We are now look for a suitable chip for our application. The STM32H747 has 4 ch I2C. Can I assign one I2C bus on CM4 core and another I2C bus on CM7 and these two I2C buses will talk to different system.Thanks,

AFung.1 by Associate II
  • 1648 Views
  • 4 replies
  • 0 kudos

STM32G071/G081 stucked bit into unique ID?

I need to have a unique ID on 32bits. Unique ID of STM32G0x is on 96bits.It may have some stucked bit for '0', for example for XY wafer position, maybe others (lot #)?I've seen that " exact information about valid bits not fixed to 0 for given deciv...

THAUS.1 by Associate
  • 2590 Views
  • 5 replies
  • 0 kudos

UART with STM32F4xx Using USB to TTL Converter

I want to do UART by connecting USB to TTL converter(PN-USBTTL-FT, FTDI FT232RL) to Tx and Rx of the board pin without using the USB port of the debugger part of STM32F4xx.The main code is as follows:uint8_t a = 'a'; while (1) { HAL_UART_Transmit(&...

GKim.1 by Associate
  • 1929 Views
  • 1 replies
  • 0 kudos