STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L475VGT6 ADC values getting stuck during ESD testing

During ESD testing, we are noticing issues with our ADC values getting stuck.We are using STM32L475VGT6.No permanent damage has been observed. Resetting the MCU always results in normal behavior.  We are using DMA to load all ADC channels.  We are ca...

PTana by Associate II
  • 4187 Views
  • 6 replies
  • 1 kudos

Does DMA miss data while it is used by SAI interface?

Hi everyone,I work on Data Acquisition System project. Our main controller is STM32F765VG. We used ADS131A0x A/D converter (by SPI) to sample input signal in our previous version. Now we want to replace ADS131A0x with ADS1274 (because of its higher s...

0693W000000UhtJQAS.jpg 0693W000000UhuHQAS.jpg
Ltura.1 by Associate
  • 1432 Views
  • 2 replies
  • 0 kudos

ADC calibration on the reference voltage

Hello I am exploring the ADC functionality of STM32F103C8T6. I connected a potentiometer to PA2 and connected an LED at PA0 as indicator. The indicator shall get activated once the potentiometer reaches the set threshold. I tried to set the maximu...

RSy.1 by Associate III
  • 1886 Views
  • 5 replies
  • 0 kudos

Using STM32 to replace old peripheral chip but it needs 8-bit parallel data bus to communicate with the Core like 8051

Can STM32 able to replace an old peripheral that required 8-bit parallel data bus and communicate between 8051 MCU. We can't modify the 8051 MCU and we can't use FPGA too. I know FSMC is very close solution to my case but in my situation, the STM32 i...

Resolved! GPIO pin does not stay high

Hi everyone,I am trying to use CubeMX and the HAL library to get two STM32F411E discovery boards to communicate with each other via SPI. In a first step I am simply trying to configure the master correctly. I want to drive the NSS pin of the slave wi...

BKölz.1 by Associate
  • 4710 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L43KC: Changing Clock Frequency?

Hey guys, just having the hardest of times changing clock frequency to 80MHz for the system clock and 43MHz for the ADC clock. Every time I try it seems the writing function to registers gets disabled such as RCC->AHB2ENR trying to enable GPIOA and A...

CLeo.1 by Senior II
  • 1779 Views
  • 5 replies
  • 1 kudos

Resolved! WFE examples required for stm32 family?

Hello ,I would like to get some examples for WFE based sleep . In stm32cube examples, i see that most of them are like WFI based examples. Request someone to help me with this information. Thanks in advance.Regards,Vinoth

STM32H745 DMA Mem-to-Mem inter-core data transfer

I would like to perform DMA based memory to memory transfer between cores with interrupt generation on Transfer Complete. To start of with the project i used Demo code (STM32Cube_FW_H7_V1.7.0 -> Projects -> NUCLEO-H745ZI-Q-> Demonstrations) added mem...

Madhan by Associate II
  • 1336 Views
  • 1 replies
  • 0 kudos