User Activity

Several questions:1. Dimensions of smallest object that can be detected.2. Maximum Sampling rate (60Hz). Can sampling time be adjusted for multiple sensor array.3. Plan to use multiple sensors. What pattern should I use to place the sensors?4. Can in...
STBOX1_PRINTF does not appear to support format %f ? using STM32CUBE IDE 1.0.2
Is there a recommended way to merge two projects? I have tried this in the past and become frustrated quickly. The mapping from the file system to the tree structure is confusing. I also have problems with include files and paths. Is there a best pra...