STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! question about stm32h750bdk ExtMem_boot

 Inside the QSPI_EnableMemoryMappedMode function, the dummy cycles are MT25TL01G_DUMMY_CYCLES_READ_QUAD_DTR - 1.MT25TL01G_DUMMY_CYCLES_READ_QUAD_DTR is defined as 6U.The datasheet for MT25TL01G states that the DTR QUAD INPUT/OUTPUT FAST READ value is...

taeun by Associate II
  • 2389 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F105RC USB Device not detected

Hello.  I have a custom board with F105RCT7. The summary of my problem is the USB interface is not working at all. The computer does not detect anyting. The board is configured as a VCP device. I have a Nucleo-H743ZI-2 board and done some tests with....

hckar_0-1747988544280.png Cattura.PNG
hckar by Associate II
  • 2677 Views
  • 5 replies
  • 1 kudos

STM32U5: ADF1 plus LPDMA plus SDMMC

I've been working on a custom STM32U595 board which uses ADF1 to read from a digital MEMS microphone and store audio samples in a SRAM4 buffer using the LPDMA. A circular buffer is implemented where LPDMA1 reads samples from ADF1 and generates interr...

coppercrimp_0-1748273140610.png

Inconsistent boot with STM32L412

Hello.I'm struggling to get a plain STM32L412KBT6 to boot consistently into the user program. I'm working with the PlatformIO environment in VSCode. I've tried both the STM32-Cube, and the Arduino framework with similar results. Here is my platformio...

po4gYhfg.png viwHjro7.png FTFwaBVo.png
JesFo by Associate II
  • 4200 Views
  • 11 replies
  • 6 kudos

Resolved! Trying to run the ADC with DMA on STM32H755ZI-Q

Hi,I a using a NUCLEO-H755ZI-Q on STMCubeide 1.18.0i am trying to use the Timer 1 to capture on the rising edge using the analog to digital converter those are my signals the lase one (pink is my signal that i want to capture at this frequency)those ...

William133467_1-1748057361673.png William133467_2-1748057954527.png William133467_3-1748058016884.png William133467_4-1748058563086.png

STM32F756ZGT6 - short circuit issue

I am facing a short circuit issue on my custom board, which uses the STM32F756ZGT6 microcontroller. The enabled peripherals on the board include USB, SD CARD, ETHERNET, UART, SPI, and I2C.This is the second time I have encountered this issue on my cu...