STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Correct value of systick

Hello everyone, I write here to know if someone can help me,how to be sure the systick value is good ? be sure that 5 seconds are well done ?thanks to help me !

ABras.1 by Associate II
  • 2408 Views
  • 4 replies
  • 0 kudos

STM32F401RE Board PWM doesn't work on this port

Hi everyoneI have an STM32F401RE board and I have an LED from pin PB6 to GND.In the same project that this snippet code below comes from I have a PWM running on PA5 pin and it is blinking.I have been at this all night and I can't figure out why PB6 i...

CMcC.1 by Associate II
  • 1890 Views
  • 5 replies
  • 0 kudos

STM32F401 plus VL53L1X crashes after 10 mins

Hi Guys,I'm using an STM32F401 board, accompanied an expansion board, and by a VL53L1X (people counter) sensor. It works for 10minutes then the board crashes and the only way to get it working again is by resetting the board.Hi Guys, What I'm usingST...

AElek.1 by Associate
  • 1058 Views
  • 0 replies
  • 0 kudos

stm32l010 analog watchdog

Can the analog watchdog work with oversampling? If so, will it monitor only the converted values after a full oversampling cycle?

adaniel by Associate III
  • 1223 Views
  • 2 replies
  • 0 kudos

unexpected reset after changing the GPIO mode on Fly.

Dear experts, my STM32F042G6 is unexpectedly reset after I switched on fly CAN_TX GPIO to output GPIO pin.  for this I did this steps.1).HAL_CAN_STOP() and then  2). GPIOA->MODER &= ~((U32) "pinX");   GPIOA->MODER|= ~(U32) "pinX");I have also made th...

RHeza.1 by Associate
  • 1347 Views
  • 2 replies
  • 0 kudos

Cannot use SPI TSIZE in Simplex receive only mode on STM32H7 ?

A question about this sentence of STM32H7 reference manual:Receive-only mode: COMM[1:0]=10In master mode, the MOSI output is disabled and may be used as GPIO. The clocksignal is generated continuously as long as the SPI is enabled and the CSTART bit ...

Gpeti by Senior II
  • 714 Views
  • 0 replies
  • 0 kudos