STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f072 external interrupts more than one

In my project am using A mcu , and wanted to use pA0 and Pc13 as two interrupt.​But interrupt for pA0 is not coming and Pc13 is coming.​Please help to know the cause.​Rohit+91-8141616356​

RKade.1 by Associate III
  • 2477 Views
  • 9 replies
  • 1 kudos

How do I get my flash programmer to reset an STM32G070 after programming it, so that I do not need to cycle power to run the just-download code?

I've tried using IAR and the Segger Flasher to program an STM32G070. However, neither programmer will reset the MCU, so that I do not need to cycle power to run the just-download code? I've seemingly tried every type of Reset. What am I missing?

DBroo.1 by Associate III
  • 3243 Views
  • 3 replies
  • 0 kudos

i use the stm32h750b-dk\demonstrations\toughgfx\mdk-arm\project.uvproj perform assembly, no issue. then perform Download, i increase the ram for alogorithm size, and add MT25L01G_STM32H750B-Disco, erase - > programming - > verify. All ok, no issue.

i use the stm32h750b-dk\demonstrations\toughgfx\mdk-arm\project.uvproj perform assembly, no issue. then perform Download, i increase the ram for alogorithm size, and add MT25L01G_STM32H750B-Disco, erase - > programming - > verify. All OK, no issue. b...

KLau.1 by Associate II
  • 706 Views
  • 0 replies
  • 0 kudos

I got an error '' over-current FW protection not supported by power stage '' when i use NUCLEO-G431RB + STEVAL-CTM009V1 + workbench

Hello,I am working on a motor control application with the NUCLEO-G431 and STEVAL-CTM009V1 boards. I try to generate the code by using control workbench, but it's doesn't work. I got an error '' over-current FW protection not supported by power s...

RBouh.1 by Associate
  • 1101 Views
  • 0 replies
  • 1 kudos

Iar compiler for stm32f

Hi,​Am using Iar IDE for stm32f072rbt6 mcu, please help to know how to check if me controllers ram and ROM and data memory is filled to what level.​Also I want to check,if my heap and stack memory is filled or not?​​Please share how to check, how muc...

RKade.1 by Associate III
  • 2181 Views
  • 6 replies
  • 0 kudos

Do STM32-Nucleo boards support intrfacing LIDAR (RPLIDAR, YDLIDAR) modules with embedded ROS? Or do we need to interface the Nucleo MCU board with a SBC like Raspberry Pi to talk to LIDAR?

I have a prototyping project to make a wheeled-robot maneuver with LIDAR using SLAM algorithm. So, can I use a Nucleo-board to control a LIDAR device with embedded ROS without the need of a SBC like Raspberry Pi? Please refer to the image attached.

ThiruV by Associate II
  • 6533 Views
  • 6 replies
  • 0 kudos