User Activity

Hello all,I've recently been trying to make the LSM6DSOX run ultra-low-power. However, I can't get it to work. I tried it with the 109V3 dev board in Unico, where I can get it to run at ~15uA. However, when I turn that configuration into a .h (header...
Hello,I've made a project with an Nucleo L011K4 where the L011K4 initializes, and then should go to sleep. It should wake up when an Interrupt is received on A2-pin.My current project is developed using the CubeMX suite. This generates standard code ...
I am looking to get a good power consumption measurement of my STM32L011K4. I bought the Nucleo-LPM01A for that. However, the project I've loaded onto my L011K4 does not load when in USB mode. I've checked the user manual UM2243, but that described o...
Hey!After doing some work I connected a Nucleo-L011K4 to the STEVAL-MKI197V1 breakout sensor board with the LSM6DSOX. I am connected through SPI, loaded the configuration (header file) on it and get it running. I've also set up a GPIO on the Nucleo b...
I wanted to initialise the LSM6DSOX on the L011K4. I've generated code through CubeMX and Set the SPI pins for it. However, I don't know how to proceed further, since I don't find any ways to port code from the MKSBOX1V1 to the current project. Are t...
Kudos from