User Activity

Is it possible for any of the analog watchdogs of ADC1 to be used to trigger TIM8? I would like to stop a PWM generated using TIM8 when an ADC1 conversion crosses a threshold. Table 251, Interconnect to the tim_etr input multiplexer seems to indicate...
I would like to use four TIM1_BKIN pins with timer 1 such that if any one of the four break inputs is active, the timer outputs are disabled. I.e. if multiple pins are configured to be TIM1_BKIN, are all of the inputs OR'd together? This would elimin...
Hi,I would like to get some clarification on the maximum STM32G4 ADC clock frequency. In the STM32G473xB datasheet (DS12712 Rev 2), on page 138 it shows a max fADC of 60 MHz for Range 1, single ADC operation. What exactly is meant by "single ADC oper...
The pdf file of the STM32G431 datasheet (DS12589 Rev 2) has an incorrect Title and Subject (it uses 474 instead of 431). My pdf viewer (evince) shows the following:Title: Datasheet - STM32G474xB STM32G474xC STM32G474xE - Arm® Cortex®-M4 32b MCU+FPU,...
The datasheet for the STM32G431 (DS12589 Rev 2) shows that the I2C3 peripheral is available on pins PC8 and PC9, but on page 206 of AN2606 Rev 42 it says that the bootloader is using PC6 and PC7 for I2C3. Since STM32CubeMX 5.5.0 agrees with the data...
Kudos from