cancel
Showing results for 
Search instead for 
Did you mean: 

how to read an analog input received from a sensor on the STM32F746 Discovery board .

Saif Eddine Dkhilali
Associate II

I want to configure the ADC / DMA to read an analog input on STM32 CubeMX, but all pins which are available on the card are not linked to an "ADC _input" :sad_but_relieved_face: .

should i use "analog_input "?

how does it works?

any help/advice is greatly appreciated :smiling_face_with_heart_eyes: .

Thanks in advance !

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Piranha
Chief II

All of the six analog inputs on CN5 are connected to ADC3.

it's done ! thanks :grinning_face: