STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Automated ADC calibration on STM32F4 ?

AN2834 Rev 4, point 4.2.9 Temperature-effect compensation says:One method is be to fully characterize the offset and gain drift and provide a lookup table in memory to correct measurement according to temperature change. This calibration involves add...

pr by Associate III
  • 5457 Views
  • 2 replies
  • 0 kudos

Resolved! 'F303 write protection, how does it work?

Reading Embedded Flash memory chapter of RM0316 and can't grab how the write protection is supposed to work.a) 4.3.2 Write protection says:It is activated by configuring the WRP[1:0] option bytesEach other instances where WRP is mentioned says i'ts e...

Resolved! STM32G474RE - I2C always busy flag

I have generated the I2C code using cube-mx. My slave device is I2C based DIGI-POT. when I check with HAL_I2C_IsDeviceReady() function - it is always coming busy flag.These below are the Hardware and Firmware checks I have done:HW checks -DIGIPOT i...

mani s by Associate III
  • 2319 Views
  • 2 replies
  • 0 kudos

How to write a parser for UART 'control packets'?

Hi allI've just jumped on the STM32 bandwagon so apologies if this post isn't in the right place. Just let me know and I'll go annoy the right people :)I've done some work with the ATMega AVR range, both via Arduino and native so I'm not a complete n...

TGilc.1 by Associate II
  • 6854 Views
  • 6 replies
  • 0 kudos

EXTI_IRQ performance on external flash

Hello there!I'm working on a custom project, using STM32H750VB with the main app running on an external flash (developed on TrueStudio and HAL 1.7.0). I'm using two EXTI pins to get the data from a RFID reader, using Wiegand 34 protocol. Basically th...

Peaga by Senior
  • 1340 Views
  • 3 replies
  • 0 kudos