STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN Bus DATA IS NOT GETTING RECEIVE NOT BY POLLING NOR Rx NOTIFICATION INTERRUPT ITS STUCKs IN TO "HAL_CAN_GetRxMessage(&hcan1,CAN_RX_FIFO0,&Rx_Header,Rx_Data);" if this receive API we are using polling mode instead of interrupt one

As per CAN new API i have implemented as followed sequence:-MX_CAN1_Init();CAN_filterConfig(); if (HAL_CAN_Start(&hcan1) != HAL_OK) { Error_Handler(); } if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_FULL |CAN_IT_TX_MAILBOX_EMPTY) != HAL_O...

Why Flash is not erased Properly using HAL API? What would be the flash value after erasing? should it return 0xFF?

I am working on STM32H743 series, and I want to do Write operation continuously. When the flash is erased by STM32CubeProgrammer it returns 0xFF, but after erasing with HAL API (HAL_FLASHEx_Erase()), I got the value other than 0xFF (i.e previously fl...

STura.1 by Associate II
  • 1229 Views
  • 2 replies
  • 0 kudos

STM32 I2C TXIS flag not set.

Hi I am using B-L072Z-LRWAN1 board and connected ToF sensor to I2C1 (PB8 and PB9).I am using the following I2C configuration: __HAL_RCC_I2C1_FORCE_RESET(); __HAL_RCC_I2C1_RELEASE_RESET(); I2cHandle1.Instance = ( I2C_Ty...

Problems using git with TouchGFX

Hello everyone,We are using git with TouchGFX so more than one developer can work in the same TouchGFX file. However every time we try to merge the project it get corrupted. We also tried to some the confiltc manually but it also didn't work.I would ...

FDigi by Associate III
  • 808 Views
  • 0 replies
  • 0 kudos

Stm32f401re serial port 6 issue

Hello Experts​Need some help with serial portI have been trying to communicate on serial 6 with MAX485 on Siemens V20 VFD drive.When I send command on Modbus it is received by the slave and slave responses properly as seen in my logic analyser. But w...

MSubr.2 by Associate
  • 806 Views
  • 0 replies
  • 0 kudos

1Hz interrupt from TIM3 ?

Dear Members,How can I get exactly 1Hz interrupt from TIM3 ?I use STM32F4 Discovery and looking at TIM_TimeBase Example, but I can not get exactly 1Hz yet...ThanksCode :TIM_OCInitTypeDef TIM_OCInitStructure; __IO uint16_t CCR1_Val = 54618; __IO uint...