STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer PWM Dithering for each CCRx register?

The STM32G4 series offers dithering to enhance the PWM ratio. My question is, if dithering can be used on ALL the compare channels of the same timer?Specifically, we generate a center-aligned PWM with two output compare channels 180° shifted. CCR1 an...

GAnde.1 by Associate II
  • 982 Views
  • 1 replies
  • 0 kudos

STM32 RS485 Communication does not work as expected

I have a weight cell which replies to specific frames over RS485 (cell contains its own communication protocol). Manufacturer has a software to test the cell so I connect it to my pc using a RS485 to USB converter and I am able to connect to the cell...

0693W000003Pk6SQAS.jpg 0693W000003Pk7KQAS.jpg 0693W000003Q5CqQAK.png
pbdiazam by Associate II
  • 3447 Views
  • 2 replies
  • 0 kudos

Sleep current

I am using STM32L010K4. I want to reduce the sleep current to 3uA ,But in the datasheet it is mentioned the the minimum sleep current is 1mA with all the peripherals disabled, which is a larg value  

STM32H743 Stack and Heap

Hi,I have my scatter file defined thus:// Scatter fileLR_IROM1 0x08000000 0x00200000 {   ; load region size_region ER_IROM1 0x08000000 0x00200000 { ; load address = execution address  *.o (RESET, +First)  *(InRoot$$Sections)  .ANY (+RO) } RW_IRAM2 0x...