STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Storing small data in internal flash

HI, we are working on STM32H750. in our program, we need to store 5 bytes in the internal flash. this data will be read everytime the device is powered on. the data will be changed whenever the settings are changed by the user. i.e. once in a while.M...

dv.13 by Associate II
  • 1379 Views
  • 1 replies
  • 0 kudos

RTC backup date and time

Hi,I created this function in order to store the date and time. It works !But the problem is when I load date and time, the time is the last before turning off the system.void RTC_Init(void) { /* Restore the date form backup registers */ RTC_LoadDa...

MMerc.1 by Senior
  • 2584 Views
  • 4 replies
  • 0 kudos

Resolved! using PWM with STM32L412

I have PWM setup on my STM32L412, but there is no output on the pins. I move a value to CCR1, CCR2, CCR3 but there is no output. I'm using cubeIDE to generate the HAL setup, but I notice that the timers aren't enabled, but this isn't the solution - e...

deep_rune by Associate III
  • 1596 Views
  • 3 replies
  • 0 kudos

Resolved! Why HSE is not getting ready?

Hi guys,I am using an stm32L552ZE with an NX2016SA-24MHZ-EXS00A-CS10820 oscilattor. Everithing runs as expected until i get to HSERDY waiting. I get a timeout at this part. For startup I am not running a cutom code and the HSE on code is:SET_BIT(RCC-...

CDan.1 by Associate II
  • 2875 Views
  • 4 replies
  • 0 kudos

Resolved! After erasing internal flash using st link utility when i will start storing sum data into internal flash it is going to be in hard-fault.

Hello Everyone,We are working on STM32F413RH. We are storing sum data into internal flash at some interval of time. Simple mechanism is used, first we are erasing sector and then we are writing our data into internal flash.But when we are erasing chi...

MGami.1 by Associate III
  • 1707 Views
  • 7 replies
  • 0 kudos

Where are timer outputs connected?

For instance STM32H750VBT6 has many timers, but CubeMx does not show where their outputs would go. I don't want to mess (enable all of them) an existing design just to see where timer output are.

LMI2 by Lead
  • 1803 Views
  • 6 replies
  • 0 kudos

Resolved! Is there a problem with STM32F098CC Datasheet ?

In STM32F098CC/RC/VC pin definitionsit is saying that PB4 has USART5_RX for LQFP48 but when i looked at PB4 AF's in Table 13. Alternate functions selected through GPIOA_AFR registers for port A , there is not USART5_RXand AF4 is empty(even there is n...

YAY.1 by Senior
  • 2257 Views
  • 4 replies
  • 0 kudos

DAC OUTPUT

Hi againI'm using STMG071 with 2*DAC. I need them as negative inputs to COMPx.in order to use PA4/PA5 for other purposes – I set  DAC1->MCR      =0x00030003; so DAC will not be output to the pin (PA4/PA5).Yet – as soon as DACs are enabled (DAC1->CR 0...

YWhit by Associate III
  • 1042 Views
  • 1 replies
  • 0 kudos