cancel
Showing results for 
Search instead for 
Did you mean: 

ADC power circuit

Moamen Ayman
Associate III

Hello, I am developing a circuit using STM32L4R9AI, VDD = 1.8v, VDDA&VREF+ = 3.13v, according to ST hardware design manual (I attached) for a better power filtration there should be bead between VDD and VDDA, will that create a problem given the voltages I used?

As I know bead equivalent circuit is inductor in series with small resistor so I am shorting the 2 voltage this way?

the bead I will use is BLM15BX601SN1D

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

> will that create a problem given the voltages I used?

Yes. In the case that VDD != VDDA, you don't want a ferrite bead between them. The app note suggests a ferrite bead in the case when VDD=VDDA, which is a requirement for the majority of STM32 chips, but not this family.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

> will that create a problem given the voltages I used?

Yes. In the case that VDD != VDDA, you don't want a ferrite bead between them. The app note suggests a ferrite bead in the case when VDD=VDDA, which is a requirement for the majority of STM32 chips, but not this family.

If you feel a post has answered your question, please click "Accept as Solution".