STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

More about STM32H747 ADC

I have an STM32H747i-Disco board and looking at the ADC example (which I have compiled and ran successfully)The example uses channel 18 and GPIO PA0_4 as both master and slave ADC inputs.I would like to use PA0_C and PA1_C as the two ADC inputs but I...

AStew.1 by Associate II
  • 1939 Views
  • 3 replies
  • 0 kudos

STM32H755 SDMMC1 and PLL1Q provides unstable clock signal

Hi,I'm attaching a picture of my clock configuration and Logic Analyzer (Saleae Logic Pro 8) so it is easier to see what I'm doing.I have set the SDMMC clock divide factor to 1 in the configuration tab, which should produce a divide factor of 2 in th...

TOlli by Senior
  • 4219 Views
  • 3 replies
  • 0 kudos

Resolved! Cannot configure VREF on Nucleo-64 STM32G474RE

Hi,Using STM32G474RE board (Nucleo-64). I have tried a lot of different things to configure VREFBUF and none of them have any effect.I'm outputting two voltages on DAC1 at 75% scale and 25% scale and they are always relative to approx 3.25V (which is...

TThai.1 by Associate
  • 1361 Views
  • 1 replies
  • 1 kudos

SPI_DMAAbortOnError when trying the spi example dma

Hi I am tryingthe spi dma example for stmH7 nucleo board, it is always takes me to the SPI_DMAAbortOnError function, and it looks like it is because it gives HAL_SPI_ERROR_UDR, any idea what could have caused it? For my master I am using 1Mbps clock ...

TIM2 Retriggerable Output (COMP1_Output ETR)

Hello, I am using an STM32L432KCU and I trying to use the TIM2_CH1 output as a re-triggerable output with TIM2 ETR input connected to COMP1_Output.The configuration done by STM32CubeIDE (version 1.3.0, build 5720_20200220_1053 (UTC)) is the following...

0693W000000WePZQA0.png 0693W000000WeLIQA0.png 0693W000000WeL4QAK.png
simo zz by Senior II
  • 2861 Views
  • 6 replies
  • 0 kudos

timer + ADC + DMA (ADC ISR overrun)

Hi all,I want to use timer 2 to trigger ADC function (ADC3) on STM32H743ZI2 platform. After DMA & timer starting, I stuck in HAL_ADC_IRQHandler(). /* Multimode not set or feature not available or ADC independent */ if ((hadc->Instance...

clee.10 by Associate III
  • 2562 Views
  • 3 replies
  • 0 kudos