STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Understanding STM32F103C8 AD Vref and AD range.

Do I understand the datasheet correctly when I believe the internal 2.1v reference is something internal, and the AD is still operating within VCC/3.3v as upper limit? Copilot suggested this:  // Enable ADC1 and configure itRCC->APB2ENR |= RCC_APB2EN...

pilot by Associate III
  • 5487 Views
  • 6 replies
  • 1 kudos

DMA - USART transfer Peripheral to Peripheral

Hi,I am experiencing a packet loss issue using Peripheral-to-Peripheral DMA between UARTs.While Peripheral-to-Peripheral configuration is referenced in the STM32U585's Reference Manual, it is not available in the HAL library. Therefore, the DMA is co...

lotou by Associate II
  • 1842 Views
  • 7 replies
  • 1 kudos

STM32N6570-DK XSPI flash incorrect data

Hello, I use an external flash in memory mapping mode and I have a strange problem. The application is executed from the internal RAM, while the checksum is calculated on the data from the external flash (simple summing of successive bytes in a loop)...

Artur5 by Associate III
  • 1378 Views
  • 4 replies
  • 0 kudos

Resolved! VBUS Sensing on STM32N6

Hello,I have a question regarding VBUS sensing on STM32N6.First off, I found theGuide to USB development resources on STM32https://community.st.com/t5/stm32-mcus/guide-to-usb-development-resources-on-stm32/ta-p/790803I also read AN 4879. I want to us...

Panda by Associate III
  • 1581 Views
  • 3 replies
  • 2 kudos

ST ROM Bootloader FDCAN CANBUS

The configuration:STLINK-V3SETConnected the two PCBs together via the three connectors (page 11).Attached jumper JP7 CAN_ON on MB1440 PCB (page 18).(STLINK-V3SET pages 17 & 23) & (NUCLEO-H723ZG page 37) & (Bootloader AN page 199) & (STM32H723 Manual ...

KoS by Associate
  • 17619 Views
  • 25 replies
  • 5 kudos

Nucleo-L433RC-P board with a BlueNRG-2 BLE

Hi I am testing the Nucleo-L433RC-P board with a BlueNRG-2 BLE interface. I configured the setup, but the BLE device is not being detected in the ST BLE app. Look at pic, Any modifications require are not ?   

Kumar123_0-1749551317611.png
Kumar123 by Associate III
  • 2217 Views
  • 12 replies
  • 1 kudos

Resolved! UART receive with HAL_UART_Receive_DMA

Hello everyone on the forum.I have created a UART DMA receive program with Nucle-H723.This time it is working properly, but sometimes it does not work properly.DMA set up in normal mode on UART4 RX.DMA initialization function of UART.void UART_DMA_In...

uart_dma01_02.png uart_dma02_02.png uart_dma03_02.png uart_dma04_02.png
Hey0256 by Associate II
  • 1645 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to get ADC value on STM32N6570-DK

 Hi everyone,I’m currently working with the STM32N6570-DK board and trying to read an analog signal using the  ADC1/2 INP8 channel (PB10) using the MB1280C Fanout board (Pin 13) with STMOD+ connector. However, I'm consistently getting a value around ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.