STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L412KB ADC Oversampling - Question to right bitshift

Hello,i am using ADC with DMA. In my initialization code i did the ADC calibration procedure like that: HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED); // ADC calibration VrefintCalValue = (*VREFINT_CAL_ADDR); // read out the calibratio...

ledi001 by Senior
  • 2536 Views
  • 1 replies
  • 1 kudos

File read in STM32

Hi, We are from Nagra IOT team currently working on IOT products based on STM boards.We are using SMT32L4 (B-L475E-IOT01A1).Our current requirement is putting a file in ST board - in flash preferably and read it using simple file I/O operations like ...

Asama.11 by Associate
  • 1244 Views
  • 0 replies
  • 0 kudos

looking for Model Based Development Tool

Hello ​I am looking for free MBD tool for programming. ​I think Algobuilder is good. but cpu is limited and dedicated only for mems sensors. ​I found MBD tool xcos based on Scilab. and module for cubemx, codegenator.https://atoms.scilab.org/toolbo...

kdok .1 by Associate II
  • 1246 Views
  • 0 replies
  • 0 kudos

Timer, DMA and ARR preload question

I need generate some pattern at GPIO outputs (in defined times i have to write some known combinations on outputs) as reaction on external trigger signal. I've let external signal to trigger timer (thru TRGI). I'am using TIM_CC event as DMA request w...

Pwm mode stm32

How can I use PWM output pulse in my program?Normally the PWM mode for instance for TIM1 will be generated on pin PA8, but I want to use the PWM signal internally in my code. How is it applicable?

AKh.1 by Associate II
  • 3707 Views
  • 7 replies
  • 0 kudos

Unexpected behaviour with using STM32 QSPI over HAL

I am using the QSPI (or dual-SPI) interface of the STM32L452 to create instructions for an LED driver using the HAL. I have managed to get it to work but I have to set quite absurd configuration options for the command to make it work.Here's my initi...

0693W000006EkvPQAS.png 0693W000006EkvUQAS.png
chmanie by Associate
  • 1730 Views
  • 2 replies
  • 0 kudos

How to inject your own data into the I2S line with DMA

Hi guys, as the question suggests,Mentioned by many, to fully learn how the I2S behave I must use my own valid data, so I can see what happens to it.I am having a bit of problems getting this guy to worked, I want this to implement a DMA to emulate t...

CLeo.1 by Senior II
  • 2376 Views
  • 2 replies
  • 0 kudos