STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

enable css?

I dont understand why this is a option for the mux clock selector. css is a great feature so i didnt find reasons to not enabling.In which cases i should not enable it?

JCuna.1 by Senior
  • 1302 Views
  • 1 replies
  • 0 kudos

STM32F103C8 What is CNT_INIT in General Purpose Timers?

HiFigure 120 in the reference manual RM0008 shows the control circuit in normal mode. It shows an update event using the Update Generation bit (UG). See attached figure.I am curious about the CNT_INIT bit, which is a pulse one clock cycle after the U...

0693W000006GD5oQAG.png
AAnth.1 by Senior
  • 1034 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F415RG missing bytes on UART RX

Hi,I have a board containing an STM32F415RG and another board containing an MCU from another manufacturer. Both boards are supposed to communicate with each other using RS-232 transceivers. The communication is running at 9600 baud and working well f...

TSchm.1 by Associate II
  • 5009 Views
  • 6 replies
  • 0 kudos

PWM formula timer5 not work

I'm using STM32l152 and use TIM5_Ch2 for generate pwm .My target frquency pwm is 2.85 KHz .I using these parameter:clock frequency = 32MHz htim5.Init.Prescaler = 6;  htim5.Init.Period = 100; I measured pwm on oscilloscope and I measure 2.85KHz with 5...

bfran.1 by Associate II
  • 1548 Views
  • 3 replies
  • 0 kudos

STM32H745 and SPI + DMA

Hi to all,I need to send on every TIM interrupt a packet stream to SPI1. I can't use the HAL_SPI_Transmit(...) because it is blocking....so I need to use the DMA but not in circular mode.I can not use the synchronization of DMA with lptim using DMAMU...

DMast.1 by Associate II
  • 926 Views
  • 0 replies
  • 0 kudos