cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432KC with W25Q16JV

RKuma.7.302
Associate II

Hello Team,

I want to use STM32L432KC with W25Q16. I have generated the code through CubeMx. 

I have tried to ready ID from W25Q16, and I getting 0xFF. 

When i have tried with the Arduino UNO board, it is working perfectly.

 /* SPI1 parameter configuration*/

 hspi1.Instance = SPI1;

 hspi1.Init.Mode = SPI_MODE_MASTER;

 hspi1.Init.Direction = SPI_DIRECTION_2LINES;

 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

 hspi1.Init.NSS = SPI_NSS_SOFT;

 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;

 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

 hspi1.Init.CRCPolynomial = 10;

 hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

 if (HAL_SPI_Init(&hspi1) != HAL_OK)

 {

  Error_Handler();

 }

/ /main code

void manufacturerID(void)

{

uint8_t ID[4];

int i=0;

uint8_t cmd[4] = {READ_ID_CMD,0x00,0x00,0x00};

HAL_GPIO_WritePin(SPI_SEL2_GPIO_Port,SPI_SEL2_Pin,0);

HAL_SPI_TransmitReceive(&_W25QXX_SPI,&cmd[0],&ID[0],4,10);

HAL_GPIO_WritePin(SPI_SEL2_GPIO_Port,SPI_SEL2_Pin,1);

if((ID[0] != 0xEF) | (ID[1] != 0x17))

{

Error_Handler();

}

else

{

printf("W25Qxxx ID is : ");

for(i=0;i<2;i++)

{

printf("0x%02X ",ID[i]);

}

printf("\r\n\r\n");

}

}

Please suggest me if any changes is required.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0