2020-08-06 1:55 AM
Hi, all
These months, I am using AFBoot + Linux + rootfs XIP image to download into 2MB internal flash of STM32F29-DISC. After some test, I can get the printing information of Linux on serial of Mobaxterm(home edition). But, when serial gets "/#", I cannot input "ls" command in Mobaxterm like other engineer(I am sure I have disable the control flow, and have tried some other terminal, and I even download the image of other people who had successfully used that image to list the files of Linux. But on my side, this issue always there). I don't know what happened that case.
The attached file is the printing information from Mobaxterm when I doing test. Please take a look at the last line.
Does any one can give me some advice about why I cannot input the command on Mobaxterm? Thanks
2020-08-06 3:04 AM
The last line is:
/ # [ 240.760000] random: crng init doneWhat does this have to do with the ls command?
2020-08-06 7:50 AM
Thanks for your reply.
I just want to input command, for example "ls", after Linux outputting "/#". But I cannot input any character on Mobaxterm. Even, 4 mins later, I get the message "random: crng init down", I still cannot input anything.
Some engineers in our country wrote blogs about that they had successfully got the unLinux boot information on their hardware STM32F429-DISC and could input command "ls" after ucLinux outputting "/#" to get the file list of file system.
I followed their steps, or even used their successful BIN file to download into my STM32F429-DISC, but I failed to input any command on Mobaxterm.
Same Hardware, same software, why I get the different result. this is my puzzle.
Please have a look at their successful outputting message.
2020-08-06 7:53 AM
2020-08-06 7:55 AM
Honestly who'd waste their time running full Embedded Linux on an STM32F429 ?
There were demos for uCLinux, but that was years ago, and I think EmCraft moved to more viable platforms.
2020-08-06 8:19 AM
haha... Thanks for your reply.
yes, using Afboot+ucLinux+rootfs is old approach to develop embedded system.
But, sometimes, payed a lot of time and cannot the get the hoped result, may let me disappointing, and I was blocked at the last step, maybe it is a little issue.