STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN-BUS Rx callback triggered infinitely many times.

Dear community,I have setup a can-bus system between two devices where: the first transmits a message on button press using HAL_CAN_AddTxMessage, the other one receives the message using a callback interrupt. However, the following problem arises: on...

KMoe.1 by Associate
  • 959 Views
  • 0 replies
  • 1 kudos

HAL Library Migration to SPL Library

Dear All,Am converting one code from HAL Library to SPL Library.In same am using SPI BUS , for it one of function is used which is as mentioned below:-" HAL_SPI_Transmit(&_W25QXX_SPI,pBuffer,NumByteToWrite_up_to_PageSize,100); "Same i wanted to conve...

RKade.1 by Associate III
  • 1482 Views
  • 3 replies
  • 0 kudos

Resolved! DMA's CT register is not changing after conversion

Hello,I'm trying to get multi-buffer DMA on ADC working. I modified `HAL_ADC_Start_DMA` function to use `HAL_DMAEx_MultiBufferStart_IT`instead of `HAL_DMA_Start_IT.But for some reason, M0 Completion Callback is executed multiple times before switchin...

Resolved! Flash page numbering in RM0444 and 0454 correct?

Rev. 5 of those RMs introduced dual-bank devices. According to "3.3.1 FLASH memory organization" the page numbers in bank 2 start at 256, which seems to be very odd as the PNB field in FLASH_CR has 10 bits, so one would expect 1024 instead.

Looking for a library for ESC control sequences

Hi. There is a task of displaying the menu, data input-output, editing from the terminal. I use stm32h743 communication via com port. Looked closely at the "ncurses" library, the problem with porting it to the project. I have no operating system. The...