STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Setting up SPI for AD7190 with STM32G474CE

Hi all, I am trying to setup SPI for the ADC AD7190. I am just attempting to reset the ADC after power up and then read the device ID register to check the communication. I have not been able to do that until now. I will summarize the code here and I...

SRama.1 by Associate
  • 3999 Views
  • 1 replies
  • 0 kudos

Hello everyone. I'm using a ADC with DMA. The device is stm32l073.

If the ADC is used alone without using DMA, the data conversion will be performed in the cycle described in the data sheet.However, the conversion time is doubled when using DMA.Do you know why?​Common conditions・Clock : 16MHz・​Clock Prescaler : Asyn...

R.K by Associate II
  • 1207 Views
  • 1 replies
  • 0 kudos

STM32G0 Custom Board NRST floating

Hello everyone ive been using STM32 microcontroller on custom boards for some while now, but particularly with the STM32G071G8 some boards are failing. After a few minutes, NRST seems to flicker and drop from 3V3 to 2,2, 1,7 and finally steady to aro...

0693W000005A03FQAS.png 0693W000005A03AQAS.png 0693W000005A0GnQAK.png 0693W000005A035QAC.png
BKN636 by Associate II
  • 3264 Views
  • 5 replies
  • 0 kudos

Resolved! State of GPIO after Watchdog Reset

Hello, I am using a STM32F401CE and would like to use the independent watchdog to cause a reset if the device would lock up for some reason. I have an external chip which is being controlled via GPIO and SPI from the STM32F401. When a watchdog rese...

JBlackann by Associate III
  • 1765 Views
  • 1 replies
  • 0 kudos

Hi Team, I'm using a STM32L4R5 and am wanting to store variables in SRAM2 as static variables so that they hold their value while the micro is in standby mode with SRAM2 retention enabled. What am I missing?

I've followed every tutorial/thread that i've been able to find but cannot get this to work. I've set: RAM2 (xrw) : ORIGIN = 0x20030000,  LENGTH = 64Kand .ram2_bss : { . = ALIGN(4); *(.ram2_bss) *(.ram2_bss*) } >RAM2In STM32L4R5ZITX_FLASH.ld and defi...

PLeij.1 by Associate II
  • 2324 Views
  • 5 replies
  • 0 kudos

SDIO 4 bit DMA UNKNOWN PROBLEM

This is sd_command line via logic analyzer. I'm writing 1024 bytes every second. But sd_commend do like that. And that's problem for me. If i wanna save some datas. sd_command line spoilng and locking my stm32f411 mcu's. I need help i don't understan...

0693W000007EhP0QAK.png
Vyagl.1 by Associate
  • 811 Views
  • 1 replies
  • 0 kudos

Hi ST Micro Would like to buy production qtys of STM32F205VET7 for 3 of my designs, cannot wait another year for delivery. Is this semiconductor still being produced OR do I need to re-design around it please. Scott_Davidson@Trimble.com

Suitable drop in replacements:STM32F205VET7   /original 512 KBytes flash, -40-105CSTM32F205VFT7   /768 KBytes flash, -40-105CSTM32F205VGT7   /1024KBytes flash, -40-105C

SDavi.2 by Associate
  • 892 Views
  • 1 replies
  • 0 kudos