STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read FMC NAND memory at same speed as write.

When writing to FMC NAND address, FMC_NCE goes low at beginning of first write and then only comes high at end of last write. I can write 0x1000 words at 10MHz using a 60MHz FMC kernel clock. Therefore with the minimum SETUP, WAIT, and HOLD time, it ...

SBrow.2 by Associate II
  • 2421 Views
  • 4 replies
  • 0 kudos

timer channels STM32F303x6/x8

Hi! Regarding the microcontroller STM32F303x6/x8.I have to generate 4+4 PWM waveforms. Waveforms from 1 to 4 have the same frequency but each must have different duty cycle. The waveforms from 5 to 8 have same frequency (different from the first grou...

ABarb.7 by Associate II
  • 2146 Views
  • 5 replies
  • 0 kudos

ERROR WHILE DOING SDRAM INITIALIZATION

I have connected external 16Mb SDRAM with STM32F429ZI controller.While initialization sequence of the SDRAM i am getting following error:handle_vCont_c, Failed continue threadError: Failed to set more breakpointsTarget is not responding, retrying...W...

0693W000008vv2kQAA.png
SGupt.5 by Associate II
  • 2382 Views
  • 3 replies
  • 0 kudos

where is public storage?

Hi!I am working to write my custom flash loader and i watched this course: How to create an external QSPI loaderbut i can not find "public storage". can you please tell me where it is?Thanks in advance!

AGhan.1 by Associate
  • 2568 Views
  • 5 replies
  • 0 kudos

can i get the list of Automotive grade MCU's?

List of Automotive Grade 32 Bit MCU's, should support all communication peripherals like i2c, spi,can,uart , if bluetooth inbuilt please mention that also. time lead should not exceed 8 weeks(india)

APd.1 by Associate
  • 1171 Views
  • 1 replies
  • 0 kudos

debugging M4 in STM32H7 Dual Core

Hello, I'm currently working with a STM32H757XI EVAL board, STM32CubeIDE 1.3.1 toolchain.I'm following AN5361 but without success.I tried different things like replacing /* Wait until CPU2 boots and enters in stop mode or timeout*/ // timeout = 0x...

GCoro by Associate II
  • 6088 Views
  • 3 replies
  • 3 kudos