2020-11-20 10:01 PM
I used USART interrupt for RS485 encoder communication. I send 8 bit data and encoder reply with a 16 bit data. The first 8 bits out of 16 bits are received correctly. But second 8 bits didn't get correctly. I observed receiving data using oscilloscope. By comparing received data and oscilloscope signal, I found that start bit of the second byte always missed. Therefor RDR register take the first 0 bit of the second byte as the start bit.
eg: first byte(0,1,1,0,0,0,0,1,1,1) second byte(0,1,1,0,0,0,1,0,1,1)
Bolded bits are start and stop bits. In second byte, underlined bit is taken as start bit.
Here is my code.
HAL_UART_IRQHandler(&huart2);
/* USER CODE BEGIN USART2_IRQn 1 */
UART_HandleTypeDef *huartx =&huart2;
uint32_t isr = READ_REG(huartx->Instance->ISR);
uint32_t cr1 = READ_REG(huartx->Instance->CR1);
if (__HAL_UART_GET_IT(&huart2, UART_IT_RXNE)==SET){
USART2->ISR;
RX[count] = (USART2->RDR);
count++;
if(count==2){
__HAL_UART_ENABLE_IT(&huart2, UART_IT_TXE);
count=0;
}
}
if(HAL_RS485Ex_Init(&huart2, UART_DE_POLARITY_HIGH, 1/16,1/16)==HAL_OK){
if (((isr & USART_ISR_TXE) != RESET) && ((cr1 & USART_CR1_TXEIE) != RESET)){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_4, 1); //DE ON
USART2->ISR;
USART2->TDR = TX[0];
__HAL_UART_ENABLE_IT(&huart2, UART_IT_TC);
__HAL_UART_DISABLE_IT(&huart2, UART_IT_TXE);
i=1;
}
}
if (((isr & USART_ISR_TC) != RESET) && (i==1)){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_4, 0); //DE OFF
__HAL_UART_DISABLE_IT(&huart2, UART_IT_TC);
__HAL_UART_CLEAR_FLAG(&huart2, UART_FLAG_TC);
i=0;
}
/* USER CODE END USART2_IRQn 1 */
Could anyone please help me to solve this issue
Thank you.
2020-11-20 11:43 PM
The other day I implemented RS485 using DMA like
HAL_UART_Receive_DMA( &huart1, (uint8_t*)&absa_response, sizeof(absa_response) );
// send request
HAL_GPIO_WritePin( re_port, re_pin, GPIO_PIN_SET ); // hi inactive
HAL_GPIO_WritePin( de_port, de_pin, GPIO_PIN_SET ); // hi active
static const uint8_t request = 0b00000010; // data readout absa
HAL_UART_Transmit( &huart1, (uint8_t*)&request, 1, 0 ); // no timeout, this makes function return faster
HAL_GPIO_WritePin( de_port,de_pin, GPIO_PIN_RESET );
HAL_GPIO_WritePin( re_port, re_pin, GPIO_PIN_RESET ); // lo activeand processed the response in HAL_UART_RxCpltCallback.
Works as a charme with 2500000 baud on a F0 device @ 48 MHz.
2020-11-21 1:02 AM
Which STM32? What is the primary clock?
Sounds like baudrate mismatch. Verify that the incoming data baudrate matches the expected baudrate, and verify your STM32's clock.
JW
2020-11-21 10:09 PM
Thank you for the reply. I'll try this.
2020-11-21 10:21 PM
I'm using STM32 F767zi. My SYSCLK is 180MHz and USART2 clk is 45MHz. Encoder baudrate is 38400bps and I set USART2 baudrate equals to that.
2020-11-22 2:39 AM
I mean, what's the source of clock, HSI or any other internal RC oscillator - which are imprecise and drift significantly with temperature - or crystal oscillator (HSE)?
And by verification, I mean measuring using oscilloscope or logic analyzer.
JW
2020-11-22 5:17 AM
I used HSE crystal oscillator(25MHz). I didn't verify the baud rate using oscilloscope and I'll do it.