STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I went through the homework on Linux, everything is as in the slides except that myProbe_Out says "p2p connected (Unknown MCU)".

Hello, I've managed to compile, debug and flash the code from homework onto the device (using Cube ver. 1.6) and was able to run the CubeMonitor under linux Manjaro. Everything works just fine and according to the slides, except that myProbe_Out and ...

Resolved! Is it possible to interrupt another interrupt?

This is a fairly high-level question... but just wondering whether the NVIC system is capable of interrupting an interrupt when one of higher priority comes in? Can someone point me to information on this?Thanks,Doug Burrell

DBurr by Senior
  • 2536 Views
  • 8 replies
  • 0 kudos

Resolved! Supplying voltage on VBAT pin on STM32F469I-DISCO

Hi everyone, I am currently working on a project working on a STM32F469I-DISCO. I would like to be able to use the embedded RTC as well as the backup SRAM. I have seen on the schematic that the VBAT pin is tied up to the 3.3V. Is there a way to still...

NKieg.1 by Associate III
  • 2815 Views
  • 7 replies
  • 0 kudos

Discrepancy chip marking vs product/chip ID ? My chip marked STM32F100V8T6B give a productID 0x414, while I expected 0x420. Have I received a batch of chips with an incorrect marking?

According to AN2606 rev 14, pid 0x414 mean high-density device, pid 0x420 mean medium-density device. We just bought 500 STM32F100V8T6B. They are deployed in an existing modular product that programs the uC in-situ. The program relies on the PID to ...

BNoss.1 by Associate II
  • 8023 Views
  • 15 replies
  • 0 kudos

STM32F072-EVAL- In this I am using given UART Example with Board in STM32Cube_FW_F0_V1.11.0 firmware. I am using RealTerm to check UART communication. ON Real Term I am receiving Garbage Character, I tried by changing baud rate but no correct response.

STM32F072-EVAL- In this I am using given UART Example with Board in STM32Cube_FW_F0_V1.11.0 firmware.I am using RealTerm to check UART communication.ON Real Term I am receiving Garbage Character, I tried by changing baud rate but no correct response.

SDwiv.1 by Associate II
  • 1532 Views
  • 1 replies
  • 0 kudos

Resolved! What should I do If I don't have the same version of tools?

I have STM32CubeIDE, STM32CubeMonitor and STM32Cube_FW_H7 ,but they are not the same version as the required version.Some are older version and some are newer versionWhat should I do.1-Should I uninstall my already installed SW and use the "STM32H72x...

HAlzo by Senior
  • 968 Views
  • 1 replies
  • 0 kudos

SAI FS configuration

Hi,I have a design that uses a STM32H757 with an external ADC that streams data out to the SAI peripheral. The ADC is the bus master and generates the clock. The ADC data is the PCM / DSP protocol format.I setup my SAI with the free protocol configur...

0693W000008xDszQAE.jpg
TMiha by Associate II
  • 2550 Views
  • 3 replies
  • 0 kudos