STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC And LPTIM in STM32L4

Hello! I once asked a question about ADC:("adc-functionality-in-stm32f1-stm32l15x-series")Since then, the ADC has gotten much,much better, thank you!There are even versions with 16-bit. But there is still one serious problem. This is a built-in refer...

fiim by Associate III
  • 1336 Views
  • 1 replies
  • 0 kudos

Transmiter and Reciever STM32F769I-DISCOVERY

Hi, I am a bit new to the STM32. I am trying to implement one board (STM32F7) as a transmitter and another board as a receiver. The boards should be able to communicate with eachother wirelessly. Any idea how it can be done? The data is in the form ...

AAshf.1 by Associate
  • 1557 Views
  • 2 replies
  • 0 kudos

Resolved! 저는 현재 STM32F410CBT3 모�?�로 개발중�? 있습니다.

저는 현재 STM32F410CBT3 모�?�로 개발중�? 있습니다. ​FLASH MEMORY MT25Q128 모�?��?� SPI로 연결하여 메모리를 사용하려고합니다.​MT25Q128 메모리�? 1M�?�기�?� �?��?�터를 저장하고 싶습니다. ​방법�?� 있으면 알려주시기 바�?니다. 내부 RAM�?� �?�기가 작아서 1M사�?�즈�?� �?��?�터를 넣�?�수 있는 방법�?� 모르겠습니다.​빠른 답변 부�?드립니다. ​

GGIL.1 by Associate II
  • 1315 Views
  • 1 replies
  • 0 kudos

IO for hall sensor probability abnormal

I use stm32f103rbt6 for bldc motor control.I config three gpio as pulldown for hall sensor, in addition,these IOs with external 3k resistors pull to 5V.But sometimes the motor halls readback by mcu are all low level.However, in fact, motor hall is go...

xzi.1 by Associate
  • 805 Views
  • 0 replies
  • 1 kudos

Resolved! Hello, I am trying to communicate between 2 STM32G4 using FDCAN. Using Test Modes it works without a problem. When i change to Normal Mode, TX and RX dont work.

Hello, I'm trying to build a simple program to communicate between 2 microcontrollers using FDCAN. Im not using a transciever yet, just connecting TX of one Nucleo-G431KB to the RX of one Nucleo-G474RE, and vice-versa. Using the test modes, External...

LAzev.1 by Associate
  • 3455 Views
  • 1 replies
  • 0 kudos

Resolved! Example for ADC in multimode with dual DMA?

Hi, I want to use the simulataneous ADC reading with 2 DMA channels, in order to avoid overrun errors (which I'm having).I'm using the HAL and I'm having a hard time understanding when is the DMA buffer of the slave channel assigned. When multimode i...

mur by Associate III
  • 8395 Views
  • 4 replies
  • 0 kudos

STM32L4: ADC3 stops when dual ADC mode selected.

Hi,I am using STM32L476VGT3. When ADC1, ADC2 and ADC3 are configured independently, everything works fine. As soon as I write into the DUAL[4:0] bits of register ADC_CCR (common control register) to set ADC1 and ADC2 in dual mode, ADC3 stops. The dua...

MGard.2 by Associate II
  • 738 Views
  • 0 replies
  • 0 kudos