STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F437IIH6 ECC and NAND Flash size

Hello.1. Whether the hardware ECC for STM32F437IIH6 support error detection and error correction? STM32F437 is connect to NAND Flash through FMC with Bank2. Reference manual RM0090 section 37.6.6 describe it can perform 1-bit error correction and 2-b...

WLiao.1 by Associate II
  • 3959 Views
  • 7 replies
  • 0 kudos

Resolved! Idea zone has now gone?

Idea Zone no longer appears on the top menu. Is this intentional?https://community.st.com/s/ideazone

Pavel A. by Super User
  • 998 Views
  • 2 replies
  • 0 kudos

Resolved! Please, where can I find a "key_pair_generation" example code for the Discovery Kit B-L4S5_IOT01A? (STSAFE)

I tried porting the example code has been done for the Nucleo board to the B-L4S5_IOT01A but I get STSAFEA_COMMUNICATION_ERROR as result. SEE BELOWKey pair generation demonstration:  1. Generate key pair through STSAFE-A's private key slot 1  => Use ...

CMura.2 by Associate II
  • 1157 Views
  • 1 replies
  • 0 kudos

STM32L4R5 UART DTR/DSR hardware connection

Hi, I'm trying to connect my bluetooth IC Ublox ANNA-B112 to STM32L4R5 using USART line. The bluetooth IC requires DTR and DSR line but it doesn't seems like STM32 has these 2 lines on the manual. Is there any ways to implement DTR and DSR on STM32?

CYeow.1 by Associate II
  • 912 Views
  • 0 replies
  • 0 kudos

Timers break and clear behavior in general

Hello. I can't fully understand break and clear funtionality of timers on STM32. In read dasheets and tryed various options for break and clear inputs, but in general it worked in a similar way:It puts timer output to predefined state untill it overf...

EAlek.11 by Associate II
  • 2931 Views
  • 3 replies
  • 0 kudos

How to synchronize multiple microcontrollers

I have multiple devices with stm32L5 mcu playing led animations and connected via RS-485. However, when I send a command via RS-485 to start led animations, they become asynchronous. I want to use an mcu clock as reference and send it to all others m...

STM32 turning DMA on and gives odd results

I am trying to dynamically start and stop PWM and DMA which are triggered by a timer with this code: void CAM_startLineTransfer(CAM_HandleTypeDef *cam) { // init DMA while (cam->requestDataTimer->Instance->CNT <= 60) {} HAL_TIM_PWM_Start...

MJørg.2 by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos

Output Compare stay on actual voltage level

I need an output compare trigger output with toggle function, and the start/stop should be on the correct frequency. Start is ok now, Stop I like to stay on the actual volatge level (high or low)The problem now I face is when I turn off the timer wit...

dominik by Senior
  • 1450 Views
  • 2 replies
  • 0 kudos