STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DFSDM and external Sigma Delta Modulator

Hi,I currently have a STM32L4R9VI (that contains the DFSDM + DMA) and I am planning to sample an IF signal ( up to 10 MHz frequency) using an external Sigma Delta Modulator AMC1305M05 (20Msps - 20 MHz frequency - 16 bits resolution). I am not an expe...

ABouk.2 by Associate
  • 2303 Views
  • 2 replies
  • 0 kudos

Can't read mpu6050 via I2C1

HelloI can read mpu6050 via I2c1 in stm32F4Disco but I cant read mpu6050 in STM32F746 Touchgfx.All values returns 0.This is my reading code. it is working in 32F4DISCO:#define MPU6050_ADDR 0xD0     #define SMPLRT_DIV_REG 0x19 #define GYRO_CONFIG_REG...

0693W00000ANlkqQAD.png 0693W00000ANlkvQAD.png 0693W00000ANll0QAD.jpg 0693W00000ANlkWQAT.png
FLine.1 by Associate II
  • 2006 Views
  • 1 replies
  • 0 kudos

Resolved! Getting Junk data on I2C LCD 16x2 display while interfacing with stm32f401re Micro controller . please help

Interfaced i2c_lcd with stm32f401re and try to program without any library .but getting junk data always,tried changing delay but same. void I2C_WriteData(uint32_t data){ uint8_t data1=0,data2=0,data3=0,data4=0;   data1= data & 0x000000ff;  data2= ...

0693W00000AN7W0QAL.jpg
Nchun.1 by Senior
  • 2042 Views
  • 2 replies
  • 0 kudos

Resolved! Confused about DMA and Cache on STM32 H7 devices.

While I was looking for H7 DMA data,​I saw the article below that DMA is not working on the H7 device.https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices​Solution 1 from that article is shown below.​--------------------------...

Resolved! STM32H7 SAI DMA; Transfer Error

/* Peripheral DMA init*/ hdma_sai1_a.Instance = DMA1_Stream0; hdma_sai1_a.Init.Request = DMA_REQUEST_SAI1_A; hdma_sai1_a.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_sai1_a.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sai1_a.Init.M...

0693W00000ANn8jQAD.png
CFran.1 by Associate II
  • 2977 Views
  • 5 replies
  • 0 kudos

Resolved! Timer Capture code not working

Hi All,To get around a problem I was having with timer capture using DMA (another topic) I changed my timer code to use interrupts. The seems to work when I debug step through it but not when I run. I am using TIM8 in input capture mode for CH1 and C...

BTrem.1 by Senior II
  • 1876 Views
  • 2 replies
  • 1 kudos

Resolved! What is the internal clock CK_INT for the STM32H7 timers?

The STM32H743 datasheet says nothing about clocking the timers. Reference manual has a chapter dedicated to each timer's counter clocking. For each type of timer the only clock is so called "Internal Clock" CK_INT . What is it? Opened my project's Cu...

eBirdman by Senior II
  • 6782 Views
  • 6 replies
  • 4 kudos

External interrupt Handler does not execute

Hi, I'm trying to execute an interrupt with the pin PCO with stm32f303re Nucleo board, but the interrupt routine never executes, actually, it just stops the program. this is my configuration code for the interrupt: //set gpioc 0 as interrupt _...

0693W00000ANkrMQAT.png 0693W00000ANkrgQAD.png

STM32F030C8T6. Reboot problem with high temperature.

I have this sentence and please give me a feedback that is it true or not true."The problem was that DTS had what appeared to be a bad batch of STM32F030C8T6 processors that would fail to reboot after a power off/on cycle once they reached higher tem...

RMach.1 by Associate II
  • 2617 Views
  • 6 replies
  • 0 kudos