STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pin to pin STM32F030R8T6 and with bigger flash size?

For our old product, we use STM32F030R8T6 chip, it only has 64K flash, but now, we add some new function on the product, so the flash size can not meet our requirement, we want more big size of flash, but we do not want to change our PCB board. Is th...

Xwang.41 by Associate II
  • 1734 Views
  • 3 replies
  • 0 kudos

Embedded ARM assembly compile error on STm32F4

Hello, I'm working on a library for nucleo F401RE board, with LL library, I'm trying to add some embedded ARM assembly code as written in the guide of arm Developer web site:__asm return-type function-name(parameter-list) { // ARM/Thumb/Thumb-...

CCont.1 by Associate II
  • 2976 Views
  • 4 replies
  • 0 kudos

STM32H723 TIM PWM first pulse wrong

Hi all,I am facing a very weird issue with PWM on my STM32H723.I am generating a very fast PWM with TIM3 (TIMx_ARR = 10, TIMx_CCRx = 5, Timer Clk 275 MHz). However, the very first pulse is clearly way too long:Does anyone have an Idea where this come...

0693W00000ANqZdQAL.png 0693W00000ANqaMQAT.png
FFunk.2 by Associate II
  • 964 Views
  • 1 replies
  • 0 kudos

DMAMUX experiment on stm32H7 with adc's and Gpio's

In one application I am currently developing I have a single pin for an adc input and an analog external mux(4051) on three pins that changes which of my actual 8 adc's is wired on this pin.I would like to iterate over the 8 different mux values and ...

SMour.1 by Associate III
  • 1498 Views
  • 0 replies
  • 2 kudos

We would like to upgrade our PCB with a more recent STM32 chip. Could you please recommend us which chip of the STM32 family is compatible or closer to the old ST10F269?

Dear ST Community,We have an old PCB with a ST10F269 chip on it.We would like to upgrade our PCB with a more recent STM32 chip.Could you please recommend us which chip of the STM32 family is compatible or closer to the old ST10F269? We want to apply ...

HTate.1 by Associate
  • 1553 Views
  • 2 replies
  • 0 kudos

Resolved! DFSDM and external Sigma Delta Modulator

Hi,I currently have a STM32L4R9VI (that contains the DFSDM + DMA) and I am planning to sample an IF signal ( up to 10 MHz frequency) using an external Sigma Delta Modulator AMC1305M05 (20Msps - 20 MHz frequency - 16 bits resolution). I am not an expe...

ABouk.2 by Associate
  • 2300 Views
  • 2 replies
  • 0 kudos

Can't read mpu6050 via I2C1

HelloI can read mpu6050 via I2c1 in stm32F4Disco but I cant read mpu6050 in STM32F746 Touchgfx.All values returns 0.This is my reading code. it is working in 32F4DISCO:#define MPU6050_ADDR 0xD0     #define SMPLRT_DIV_REG 0x19 #define GYRO_CONFIG_REG...

0693W00000ANlkqQAD.png 0693W00000ANlkvQAD.png 0693W00000ANll0QAD.jpg 0693W00000ANlkWQAT.png
FLine.1 by Associate II
  • 2002 Views
  • 1 replies
  • 0 kudos