STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to determine CPU load stm32h743?

Hi.I need to estimate the cpu load and output the data as a percentage to a variable ram and to an LED. I use stm 32h 743. The microcontroller works without sleep. It is advisable to make accounting and interruptions. Can you suggest a solution?

F103: User Flash program runs happily despite BOOT0=1

I would assume it should start the system bootloader. Instead, my app which is blinking a heartbeat runs happily.When I put also BOOT1=1, system should boot from SRAM and because nothing's there, the LED should remain off. Which it does.So why does m...

Peta_rj by Associate II
  • 1400 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F072RB part no unavailability.

I am looking for STM32F072RB part no but currently it is out of stock and not available anywhere. Can somebody provide alternative part no which is available easily.Please share the source details .Any help would be helpful. Thank you. 

STAR by Associate II
  • 1741 Views
  • 2 replies
  • 0 kudos