STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! C++ for firmware development - how do I get started?

I have decided to implement my firmware in C++ on an STM32 Arm Cortex M4 microcontroller. However, I find it difficult to get started. I lack good examples and learning tools.Does anyone know good examples of firmware in C++?

CH_bot_ by Associate II
  • 6592 Views
  • 4 replies
  • 0 kudos

Resolved! Is it possible to Connect an STM32H745ZI-Q(after configuring the CAN Engine) to a CAN Bus operated at 24 Volts?

Hello ST Community and Experts, I have an STM32STM32H745ZI and i have programmed it to send and receive some CAN messages from an other STM32 F446RE Nucleo Board. I would like to know if i can use STM32STM32H745ZI to connect to a different CAN Busno...

KA by Associate II
  • 1685 Views
  • 2 replies
  • 0 kudos

Resolved! Executing code with stm32f469 from SDRAM

Hi, My board consists of stm32f469 that interfaces SDRAM via FMC. I want to execute code from SDRAM. Code is loaded from internal flash to SDRAM at address 0xc0000000. But running the code from this region causes hard-fault. Is there a restriction wi...

ari_v2 by Senior
  • 3407 Views
  • 6 replies
  • 0 kudos

Resolved! How to detect STM32F417 MCU reset source

I try implement a function to detect how the MCU start from, reset from watchdog or hardfault or recycle power.Watchdog reset, if the code goes to dead loop, it will trigger WD, but I have no good idea how to capture it.Recycle power, I can use PVD_I...

STM32F7: Is it possible to generate PWM signal based on external freq source (not clock src!) using timer's external input trigger?

Hello,I've not much experience with all STM timer modes. I have a DDS-based freq source which produces meander wave. On base of this src I want to produce PWM signal using STM timer. As I understand, a regular way to do it is to pass the DDS src as e...

Wowa by Associate III
  • 2641 Views
  • 4 replies
  • 0 kudos

Power Supply Scheme capacitor STM32F030

Hello, the datasheet of STM32F030C8 say to use 100nF and 4,7uF capacitor. I have a doubt about the type of this 4,7uF capacitor. I have to use a ceramic, tantalum ou electrolytic? If I use a ceramic, this need a specific model or any ceramic capacito...

0693W00000APuBjQAL.jpg 0693W00000APuCmQAL.jpg
Rogerio by Associate
  • 1498 Views
  • 1 replies
  • 0 kudos