STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need to control RTS and CTS

Hello community,I need to control RTS and CTS signals in my application.But, It looks like STM internally controls these signals.Can anyone suggest better way to control them in my application.Thanks,Hiren Bhuva

Using SEGGER system view with STM32F767ZI Nucleo board ?

Hi Guys ! I am trying to record the activity of my MCU running RTOS . I am currently in efforts to integrate the segger system view for this particular usage. I am currently stuck in the process of RTOS Patching error . Can anyone provide suggestions...

0693W00000BaHf2QAF.png
SSRIN.1 by Associate III
  • 745 Views
  • 0 replies
  • 0 kudos

STM32F3 DMA triggered by ADC triggered by TIM without HAL

Hello,currently I'am working on a STM32 project with the CMSIS core. I want the ADC getting triggered by a Timer (TIM3). Iam trying to do that with the TRGO option.The ADC should sample 4 different channels. Each channel then gets transfered by the D...

MF.3 by Associate
  • 1499 Views
  • 1 replies
  • 0 kudos

Weirdest thing happening with STM32H7 I2S hardware

Hi guys! I am having the biggest issue with the I2S right nowWhat is happening: For whatever reason the I2S does not want to transmit any samples VIA DMA. Doesnt matter what I do what I try.The weird thing happening: The I2S WS, SCLK wont work. Only ...

CLeo.1 by Senior II
  • 6398 Views
  • 25 replies
  • 0 kudos

UART not receiving NULL hex bytes on STM32F103C8T6.

I'm using STM32F103C8T6 processor with an 8MHz internal clock, 9600 baud rate, 8bit + 1stop bit and no parity. For receiving uart data, I'm using a global interrupt. While I'm receiving data with usart1 or usart2, I can not receive null bytes. Now I ...

0693W00000BaCIwQAN.jpg
BJako.1 by Associate II
  • 3171 Views
  • 7 replies
  • 0 kudos