Skip to main content
RLind.2
Associate II
February 3, 2021
Question

Why does the first debug-usart-init work and not the second?

  • February 3, 2021
  • 1 reply
  • 587 views
#include "stm32f4xx_hal.h"
static UART_HandleTypeDef UartHandle;
 
void Setup( void ) {
 GPIO_InitTypeDef GPIO_InitStruct;
 
 
 /* STM32F4xx HAL library initialization:
 - Configure the Flash prefetch, instruction and Data caches
 - Configure the Systick to generate an interrupt each 1 msec
 - Set NVIC Group Priority to 4
 - Global MSP (MCU Support Package) initialization
 */
 HAL_Init();
 
 SystemClock_Config(); /* Configure the system clock to 180 MHz */
 
#if 0
 // **** THIS WORKS ****
 // Nucleo DEBUG = PA2/AF7/USART2
 __HAL_RCC_GPIOA_CLK_ENABLE();
 GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); // PA2 = TxD2, PA3 = RxD2, AF7
 
 UartHandle.Instance = USART2;
 UartHandle.Init.BaudRate = 38400;
 UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
 UartHandle.Init.StopBits = UART_STOPBITS_1;
 UartHandle.Init.Parity = UART_PARITY_NONE;
 UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 UartHandle.Init.Mode = UART_MODE_TX_RX;
 UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
 if(HAL_UART_Init(&UartHandle) != HAL_OK) Error_Handler();
#else
 // **** This does NOT work ****
 // Display debug = PC10/AF7/USART3
 __HAL_RCC_GPIOC_CLK_ENABLE();
 GPIO_InitStruct.Pin = GPIO_PIN_10 | GPIO_PIN_11;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); // PC10 = TxD3, PC11 = RxD3, AF7
 
 UartHandle.Instance = USART3;
 UartHandle.Init.BaudRate = 38400;
 UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
 UartHandle.Init.StopBits = UART_STOPBITS_1;
 UartHandle.Init.Parity = UART_PARITY_NONE;
 UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 UartHandle.Init.Mode = UART_MODE_TX_RX;
 UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
 if(HAL_UART_Init(&UartHandle) != HAL_OK) Error_Handler();
#endif
}

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
February 3, 2021

You enable the USART clocks somewhere?

Check the registers, RCC, GPIO and USART..

Still not working check the board, scope the pins.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..