STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Timer event in foreground vs hardware Timer

I've a colleague who is using the 32-bit timer of an STM32 to trigger and interrupt handled pin toggle rather than using the 16-bit hardware Timer on the pin that needs toggling. The frequency on that pin varies a lot in use. When I wrote bringup cod...

Chris Pad by Associate II
  • 8942 Views
  • 20 replies
  • 0 kudos

Resolved! Are these parts counterfeit?

I am a PCB designer for a start up Medical Company. We are gearing up for our commercial launch, do to the current supply chain issues we are have trouble acquiring parts. we bought these parts from a company in Canada, they shipped from China. The t...

AHans.2 by Associate
  • 2745 Views
  • 3 replies
  • 0 kudos

About Quad SPI communication problem with Serial NAND Flash (Winbond-W25Nxx). Problem with Reading Sequence in quad I/O

Hi,I am working on Serial NAND Flash (Winbond W25Nxx) communication with H747 microcontroller. I'm having a problem with the Serial NAND Flash I have. I think this issue is related to QuadSPI structure.Reading sequence in quad I/OSerial NAND Flash co...

0693W00000BbvbRQAR.png 0693W00000BbvcZQAR.png

Can the STM32 ADC do what the PIC16F ADC can do?

I have an existing design using an 8-bit PIC16F and am attempting to upgrade it to using the STM32L071, primarily due to needing more memory. This design has 6 input signals being sampled using the same ADC. One signal is an audio signal that needs t...

BrianG by Associate II
  • 2369 Views
  • 4 replies
  • 0 kudos