STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i have written a led blinking program with as per my knowledge but i couldn't reach output so guys who can clear that? MCU- STM32f401 clock input -25MHz External clock output -80 MHz with pll configuration

#include "stm32f4xx.h"#define PLLM 25#define PLLN 320#define PLLP 1//divide 4void SysConfigure(){      RCC->CR|=RCC_CR_HSEON;//External Crystal Oscillator      while(!(RCC->CR & RCC_CR_HSERDY));// External Crystal oscillator status flag checking     ...

Msams.1 by Associate II
  • 2860 Views
  • 7 replies
  • 0 kudos

Generating 1 nanosecond update event using Timers - AN4013

According to AN4013 on using timers as time base generators, one could use a 16-bit timer to generate an update event from a nanosecond to a few minutes. Well, take for example the STM32F429 clocked @ 180 MHz. If one cycle takes 5.56 ns, which is the...

0693W00000D0FIqQAN.jpg
Zaher by Senior II
  • 5680 Views
  • 10 replies
  • 0 kudos

Modbus over RS485 with STM32F303K8

I'm looking to make a loop of MCUs as slaves to a PC master so that I can send commands to them. The idea is to use the https://www.maximintegrated.com/en/products/interface/transceivers/MAX22025.html and https://www.ftdichip.com/Support/Documents/Da...

0693W000004KPkyQAG.png 0693W000004KPrGQAW.png
RWedu.1 by Associate II
  • 9428 Views
  • 8 replies
  • 0 kudos

STM32L476 LPRun Mode external clock source Frequency

I'd like to you a STM32L476 continuesly in LPRun Mode with external Oscillator Frequency of 2.048MHz. But in "Reference Manual" of STM32L476 is written following: "5.3.2 Low-power run mode (LP run)To further reduce the consumption when the system is ...

MGehr.3 by Associate II
  • 1084 Views
  • 1 replies
  • 0 kudos

Abnormal delta of TSC after exiting STOP mode

Hi,MCU: STM32L072MCU is using TSC and ST touch sense library. Before entering stop mode, the delta of touch key without pressing is normal (-2 to 2). However, after exiting STOP mode and then calling tsl_user_Exec_IT(), there is strange value delta.B...

John_1992 by Associate II
  • 1489 Views
  • 1 replies
  • 0 kudos

STM32H743IIT6

Left side original label from MFG but there is a misspelling on the temperature.Right side label from Mouser with the correct spelling.Please advise whether it is a common error on the misspelling issue.

0693W00000BdPOAQA3.jpg
ENeoh.1 by Associate II
  • 915 Views
  • 1 replies
  • 0 kudos

QUAD SPI MT25QL128A with stm32H750Ibt6 controller.

Hello all,Currently i'm working over STM32H750IBT6 Controller with QUAD SPI MT25QL128A External flash. The objective is to boot from internal flash address which is 0x08000000 and jump to external flash address, as the internal flash memory is quite ...

Mani.V by Associate II
  • 935 Views
  • 0 replies
  • 0 kudos