STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC not maintaining the date and time as expected

I am experiencing issues with the VBAT pin on the STM32H753ZI Nucleo board. Specifically, the VBAT pin is not responding properly. I am using a CR2032 CMOS battery for RTC backup, but it is not maintaining the date and time as expected. When the powe...

Ematic_0-1753077475445.png
Ematic by Associate II
  • 1178 Views
  • 5 replies
  • 2 kudos

Flash Image integrity inquiry

Hi,I am using STM32G07 for the slave side, and another MCU for the Host side.I would like to implement the device firmware upgrade of the ST MCU, and controlled by the Host MCU.There is only support for UART communication between two MCUs.ST MCU Prot...

TesterSAM_1-1753778391814.png
TesterSAM by Associate III
  • 402 Views
  • 1 replies
  • 0 kudos

STM32H563ZI, Openocd configure and flash

Greetings! Getting back into embedded after a long while. As the title says I am wanting to use STM32H563ZI with openocd, but it is not supported out of the box. I have gone through the readme and it looks like I need to create a specific `target/stm...

tebel by Associate II
  • 7388 Views
  • 7 replies
  • 3 kudos

Resolved! STM32L073 operating on low power

Hi, I am working on a project where I have a custom board with STM32L073 MCU and I want to read a color sensor (AS7341) via I2C. This will be a low power application. I will harvest energy via NFC from a smartphone (I am using NTAG I2C plus). I can g...

sam111_0-1753287730279.png
sam111 by Associate II
  • 1501 Views
  • 9 replies
  • 3 kudos

Resolved! Unsolicited interrupts when temperature rises around 60°C

Hello,I am using a STM32L476RCT which should work up to 85°C.I am receiving unsolicited interrupts when I put my board in an environment at 60°C.I only use usart1 and a few GPIO interrupts, which are working fine. But when the temperature rises, the ...

gmaeng by Associate II
  • 969 Views
  • 7 replies
  • 5 kudos

I did not get desired response while flashing GPIO demo

I am currently working on the STM32H7S78-DK board & after building GPIO demo present Example code from git repository of that STM32 provided, while flashing binary from the STM32 programmer I faced issue it is mentioned belowWhen code is flashed from...

amar_1_0-1753364633108.png
amar_1 by Associate
  • 401 Views
  • 1 replies
  • 0 kudos