STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743VIT6 gets very hot @480 MHz

Hello all,I'm evaluating the STM32H743VIT6 on a third-party development board. I tested it with the system clock configured at 480 MHz (double checked everything, and all looks absolutely fine in terms of configuration). I did enable the "overdrive" ...

OpusOne by Associate III
  • 914 Views
  • 4 replies
  • 3 kudos

STM32G0B0REx RTC smooth calibration

Dear all, I'm calibrating the STM32G0B0RE RTC clocked by an external 32.768 oscillator using the following guide:https://community.st.com/t5/stm32-mcus/how-to-calibrate-the-stm32-s-real-time-clock-rtc/ta-p/744958Below is my debug code:int main(void) ...

Moreno_Ortolan_0-1754035040817.png

STM32G431KB DAC DMA not working

Trying to get a basic sample DAC1 with DMA, triggered by TIM2 working. This should be trivial, works fine on SMT32F3. I'm using a Nucleo-32 SMT32G431.Using Cube IDE. The only non IDE-generated code in main is: /* USER CODE BEGIN 2 */   static uint...

PBieg.1 by Associate II
  • 33114 Views
  • 23 replies
  • 4 kudos

Resolved! STM32H523 hardware development problem

Greetings. I am a beginner and an electronic student and I am currently getting my hands on STM32H523. I have created a mcu board in Altium Designer just to control LEDs by GPIO, hopefully to understand more about STM32. I have the PCB fabricated, an...

TIM One Pulse Mode

Hi all,I'm trying to get one pulse mode working on the TIM1 of the STM32H755. The goal is taking a pulse from one pin as a trigger, starting the pulse, counting 32 clock cycles on another pin, and then resetting the output. This controllers tech tuto...

noahyonr by Associate II
  • 824 Views
  • 2 replies
  • 1 kudos

stm32h563 edata Code Generation issue

Hello,On flash option byte I need to use only one sector. Only Edata bank1 is activate. No other option bytes are required.CubeMx generate MX_FLASH_Init with Edata configuration commented. What other option byte is necessary to select to use Edata on...

BenoitS by Associate
  • 3446 Views
  • 3 replies
  • 0 kudos