cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple ADC channel Poll not working

MPers.1
Associate II

Hi,

I am trying to poll multiple channels of the ADC but always get the result from channel 0.

The other channels only work if I use them one at a time.

Pretty sure it is a setting and would appreciate your help.

Thank you in advance!

Using a STM32F070.

Here is my code:

static void MX_ADC_Init(void)

{

 /* USER CODE BEGIN ADC_Init 0 */

 /* USER CODE END ADC_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC_Init 1 */

 /* USER CODE END ADC_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)

 */

 hadc.Instance = ADC1;

 hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;

 hadc.Init.Resolution = ADC_RESOLUTION_12B;

 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;

 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;

 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

 hadc.Init.LowPowerAutoWait = DISABLE;

 hadc.Init.LowPowerAutoPowerOff = DISABLE;

 hadc.Init.ContinuousConvMode = DISABLE;

 hadc.Init.DiscontinuousConvMode = DISABLE;

 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;

 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

 hadc.Init.DMAContinuousRequests = DISABLE;

 hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;

 if (HAL_ADC_Init(&hadc) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure for the selected ADC regular channel to be converted.

 */

 sConfig.Channel = ADC_CHANNEL_0;

 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;

 sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;

 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure for the selected ADC regular channel to be converted.

 */

 sConfig.Channel = ADC_CHANNEL_1;

 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure for the selected ADC regular channel to be converted.

 */

 sConfig.Channel = ADC_CHANNEL_4;

 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN ADC_Init 2 */

 /* USER CODE END ADC_Init 2 */

}

// once every second I call this function in a loop (starting with channel 0 and going up to 2)

uint16_t MX_ADC_Start(uint32_t channel)

{

ADC_ChannelConfTypeDef sConfig;

uint16_t uhADCxConvertedValue = 0;

/**Configure for the selected ADC regular channel to be converted.

*/

sConfig.Channel = channel;

sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;

sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;

if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)

{

/* Starting Error */

Error_Handler();

}

if (HAL_ADC_Start(&hadc) != HAL_OK)

{

/* Start Conversation Error */

Error_Handler();

}

if (HAL_ADC_PollForConversion(&hadc, 10) != HAL_OK)

{

/* End Of Conversion flag not set on time */

Error_Handler();

}

else

{

uhADCxConvertedValue = HAL_ADC_GetValue(&hadc);

}

return uhADCxConvertedValue;

}

//The return value is always the one from channel 0 even if I loop through all other channels as well.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

Channels are converted on order. If you want to convert channel 1, you'll need to ensure channel 0 is not selected for conversion in the CHSELR register.

If you feel a post has answered your question, please click "Accept as Solution".
MPers.1
Associate II

I thought this was done in HAL_ADC_ConfigChannel?

There the channel in binary format seems correct with 10011 ( channel 0, 1 and 4).

But this is a bitwise OR operation so the channels will not be cleared if setting another channel.

after doing this manually it worked perfectly:

hadc.Instance->CHSELR = 0;

Thank you for your help!