STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L4R: How do Flash Option DBANK and DB1M interacts?

In FLASH_OPTR, both DBANK and DB1M are r/w and have no restrictions beside that PCROPA/B needs to be disabled. For 1M device there are two(?) sensible settings DBANK=1, DB1M = 1 for 1Myte dual bank continous modeDBANK=0, DB1M = 0 for 1Myte single ban...

Implement Cordic of Arctan2 through ADC and DMA

I need to calculate angle value with input of sin/cos from ADC1/ADC2 channel by DMA way. As using the cordic of atan2 function,I think that two parameters of Y and X need to be written to pInBuff as like the key code below, is it correct? sCordicConf...

CWang.9 by Associate
  • 1134 Views
  • 0 replies
  • 0 kudos

Is five-volt tolerance guaranteed in Standby / Stop mode?

I want to wake-up from standby mode on a STM32L422xx using PA2 (WKUP4) with pull-down enabled in PWR_PDCRA. Wake-up signal can go up to 5.25V at this pin.Can this configuration cause any problems e.g. high current injection during wake-up phase?Thank...

C.Ecke by Associate
  • 798 Views
  • 1 replies
  • 0 kudos

I'm trying to use HRTIM to generate non-overlaping PWM pulses on 2 outputs, and be able to change which output is first in time. I've tried various methods and find when I change the output order, it corrupts the pulse lengths and they overlap.

Nulceo 64- F334R8. Using Timer A on HRTIM1 to generate non-overlaping PWM pulses on 2 separate outputs. I use 4 CMP registers, defining the start and end time of each pulse (CMP1 = pulse 1 start, CMP2 = pulse 1 end, CMP3 = pulse 2 start, CMP4 = puls...

ORidl.1 by Associate
  • 1880 Views
  • 2 replies
  • 0 kudos