Hello,Is it possible to connect a target board with a STM32 to a Nucleo-L432KC kit and download the firmware inside the STM32 ? The connector CN2 is only to programm the STM32F103, it's not a connector for the target ?thanks
Hi,The package UFQFPN32 (5x5 mm) have an exposed pad but where is the definition of this Exposed Pad in the datasheet for the STM32F302K8 K Must I connect to the GND or is it not connected or maybe another pin definition ? I can't see in the datashee...
Hi,So it's possible but not so easy.First thing is to disconnect the L432KC on the Nucleo board, ie JP1 must be open, like this the L432KC have no power and must be in HZ.My target need less than 40mA on the 3.3V, so I use the GND and the +3V3_ST_LIN...