STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F303RE Tim2 ch2 PWM Mode

Hi everyone, I'm trying to use the Timer2 CH2 PWM Mode 1 to generate a 1 Hz signal with 50% Duty Cycle out of my PA0 pin but i can't get anything. Here's my code:#include"stm32f3xx.h"   void TIM_PWM(void);   int main(void){ TIM_PWM(); while(1){ } }...

Nick- by Associate II
  • 2384 Views
  • 2 replies
  • 0 kudos

Resolved! How get the List file from assembler?

HelloI'm using CubeIDE.I want to get list file which is containing OP code from "Startup_stm32f427zgtx.s" as a output of assembler.I heard that I could use -Wa, -al option here and there on the Webs, but I couldn't get the list file of the assembler....

SSeo.17 by Associate III
  • 2735 Views
  • 2 replies
  • 0 kudos

STM32F3 SPI3 not working

Hey,I'm working with STM32F303RET6.I'm having trouble transmitting data with SPI3 (PB3, PB4, PB5 and PA15).Before I'll post my code here, I want to say that I am also working with SPI2 (PB12, PB13, PB14 and PB15) with the exact same configuration on ...

RLosc.1 by Associate II
  • 3245 Views
  • 5 replies
  • 0 kudos

Resolved! Circular buffer resetting start point?

I'm trying to use DMA to handle my incoming Rx data and, ideally, I'd like to just increment the index to keep track of the incoming data, essentially like this:#define uartsize 2000 #define dma_buffer_interrupt_size 1   uint8_t UART_in_Buffer[uarts...

JayDev by Senior II
  • 4031 Views
  • 2 replies
  • 0 kudos

Resolved! stm32h743 adc1 eos flag will not be set until I read the DR

Hi all, recently I am trying to use ADC to sample 4 channel current signals. Since there is no critical time requirement, I plan to use scan mode. In my opinion, the ADC will automatically complete four channel signal conversion stuff, then set the...

Whono.1 by Associate II
  • 5267 Views
  • 7 replies
  • 5 kudos

STM32L4Rxxx OctoSPI with PSRAM

Dear All,In "RM0432 Reference manual STM32L4+ Series advanced Arm ® -based 32-bit MCUs" in chapter "19.3 OCTOSPI implementation" and table "Table 119. OCTOSPI implementation" there are some differences in supported features between families. All fami...

Resolved! INVPC occurs when SVC Handler returns

I use STM32F1 Value Line Discovery Kit.​I want to write SVC handler.If I implement the following, invpc occurs when running 「POP PC�?in Line 38.Caller -------------------------------- __asm volatile(" SVC %0 \n" : : "I" (2)); ...

Myasu.1 by Senior
  • 2046 Views
  • 4 replies
  • 0 kudos