STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hi i am using nucleol073rz board , trying the IAP xmodem usart example , not able to load bin file more than 15KB cant find the problem or understand why ? whereas for code less than 15KB it is working.

Below is the code snippets , not able to debug as well i suspect the flash is not able to erase completely need some advice on this .https://github.com/ferenc-nemeth/stm32-bootloader//////////////////////////////////flash operation//////////////////...

svii by Associate III
  • 4047 Views
  • 7 replies
  • 0 kudos

ST-LINK on Nucleo-F412ZG hard reset?

I have a Nucleo-F412ZG which ST-LINK is not detected by Windows10. On first Windows10 machine, after fiddling with the drivers, it is now detected as USB Serial Device (COMX), on the second windows10 machine it is as a Jlink CDC UART Port (COMX)Neith...

mbristol by Associate II
  • 3143 Views
  • 7 replies
  • 0 kudos

ADC input and GPIO output on the same pin

Does anybody have any experience in using exactly the same pin as an ADC input and a communication GPIO (out), as two alternating functions? Would it be possible to switch between them? If so,can the GPIO drive the small capacitor that is typically n...

CObn.1 by Associate II
  • 2305 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G031FX Timer

Hi there!i try to configurate TIM14 for generate one interuupt every 1000ms just for try but dosent't work . the frequency is 16Mhz i setup a prescaler 1600-1 and the Counter period 10000, but i diden't receive any interrupt. Before the while i turn ...

SGian.1 by Senior
  • 1274 Views
  • 2 replies
  • 0 kudos

BLUENRG_LP STEVAL-IDV011V1 issue

I can’t program my STEVAL using SWD neither UART right now. My last FW only configures my accelerometer an them goes to SHUTDOWN. When the MCU is on SHUTDOWN mode I could never program STEVAL using SWD (in Keil or using BlueNRG-X-Flasher Utility), bu...

0693W00000DnPcVQAV.jpg 0693W00000DnPj1QAF.jpg
ARamí.1 by Associate II
  • 1939 Views
  • 3 replies
  • 0 kudos