STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0xx - why is PA4 initialized as digital input?

In STM32L0xx, all pins are initialized as Analog, except PA13/PA14 which are SWDIO/SWCLK, initialized as AF; and PA4, which is initialized as [digital] Input.I can't find any reason for the latter.It's not that important, and I can simply take it as ...

OTA update

I would like to know if the following is possible and if so, where can I find information about it.I have a STM32L010K8 micro connected via USART to an LTE CHIP (BG96) through which I can get the firmware update that runs on the microcontroller. I co...

YOrop.1 by Associate
  • 1943 Views
  • 2 replies
  • 0 kudos

STM32F3 - Permissible Magnetic Field Strength

I am currently using the STM32F3 series microcontroller (STM32F303CB) in a magnetic sensing application. Since the environment is prone to magnetic field, I wish to know the maximum field strength that the microcontroller can withstand.I could not fi...

MagSense by Associate II
  • 2336 Views
  • 2 replies
  • 0 kudos

Resolved! How to get the audio line-in data from the STM32H735G-DK?

I tried the BSP example for H735G-DK, but it doesn't work.What I want to do is get an audio wave from line_in (the blue audio jack on the board).The setup for SAI1 is in the picture, I can play the audio through the line out without any problem but c...

0693W00000Kde20QAB.jpg 0693W00000Kde2AQAR.jpg 0693W00000Kde2ZQAR.jpg 0693W00000Kde2VQAR.jpg
GChen.5 by Associate II
  • 2952 Views
  • 4 replies
  • 0 kudos

interface MAX1300 ADC with STM32F0 DISCOVERY through SPI

Hello,i am trying to interface MAX1300 ADC with STM32F0 DISCOVERY through SPI but not able to receive complete 16bit converted data.8-bit of data is not getting received through spi. suggest some solution to resolve this issue

pt31 by Associate
  • 1650 Views
  • 1 replies
  • 0 kudos

Can't run application with my Nucleo-144

The Nucleo is H743ZI2 (Nucleo-144).I can properly update the firmware so I guess the Nucleo is properly detected by STM32CubeIDE.I can properly build the application without errors.However, I can't run it. For some reason, the board is not detected a...

0693W00000LvTsFQAV.png
APere.10 by Associate II
  • 2116 Views
  • 6 replies
  • 0 kudos