User Activity

Hi all,I have recently started working on stm32l072 LRWAN module of stm. I was able to build and run the code as it and was also able to send data to the gateway. My next task is to interface some sensor the the controller and send the sensor data to...
Hi all,I have just started working with stm32 and i am trying to port some example code from stm32f0 to stm32l0 board.When i configured my project on L073rz board with same configs in F0 series i am getting errors for some api's available in stm32l0x...
Hi all, I am new to Lora technology and need some guidance from experts here.I am working on B-L072z LRWAN1  module that allows to transmits messages using Lora. I was able to download and flash the example code available in LRWAN library provided by...
Hi all,I have recently started working on B-L072Z-LRWAN1 for understanding the LoRaWAN protocol.I am using icube lrwan software for example code.I was able to build the code successfully.But when tried to flash the code using openocd,i am continuousl...
Hi ,I am working on STM32L0 series controller that has 3 different external interrupts configured on PB11(sensor A),PB2(Sensor B) and PC1(Sensor C).Peripheral connected to PB11 generates interrupt at 1ms interval and PB2 generates interrupt when dat...
Kudos from