STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to start STM32F767ZI Nucleo board when connected to an external 5 VDC power supply ? I set JP3 to E5V, when I switch on the 5 VDC external power, green led LD6 PWR goes on but I have to press the reset button B2 to start the program running.

Not clear if I have to remove SB111 (only if powered with 3.3 VDC according manual)So, how to make the board running its program without user intervention when it is powered via E5V (pin 6 and 8 of CN11)Thank you, J.

jea74 by Associate III
  • 1064 Views
  • 1 replies
  • 0 kudos

Auto baudrate detection STM32G0 - Error calculation

Hello,I consulted :https://www.st.com/content/st_com/en/search.html#q=usart%20stm32G0-t=products-page=1I was wondering where to find an AN describing "Error Calculation" for STM32G0Or if the below document (AN4908) is globally applicable for every pr...

Sego2 by Associate III
  • 1123 Views
  • 1 replies
  • 1 kudos

Unable to initialise interrupts || Nucleo - F746ZG

Hi everyone,I am new to the world of STM32 MCU's so please bear with me.I am following a tutorial on Udemy and trying to write a GPIO interrupt code from scratch. I have done all register configurations and config is working fine as seen through SFR ...

MShar.7 by Associate II
  • 1612 Views
  • 4 replies
  • 0 kudos

STM32F7 MCU with J-link programmer

I'm using Segger's J-Link programmer to program STM32F767 MCU. Quick Question:1) During programming/flashing (while downloading a binary file), J-Link programmer asserts RESET# line logic LOW or RESET# line will logic High?

S.Kamath by Associate III
  • 1639 Views
  • 1 replies
  • 0 kudos

How do I get Timer8 Compare to toggle an output pin?

Working with TIM8; I have enabled one-time-pulse, set 'Channel1' to 'Output Compare CH1', set the Output Compare Channel 1 Mode to 'Active Level On Match', and Pulse to 0. I set the timer's ARR = 65535, and set the Compare Register to 20000. I hav...

LMorr.3 by Senior II
  • 1718 Views
  • 2 replies
  • 0 kudos